About Project from Example —— ADC_s32k144

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About Project from Example —— ADC_s32k144

2,037件の閲覧回数
kemingkai
Contributor III

Hi NXP Engineer:

      I have a problem with Project from Example —— ADC_s32k144. In the code i see the function which (Convert chan 29, Vrefsh) at the end.

pastedImage_3.png

I want to know what is it used for?I can serach the note AN5413,and find some description and image like this 

pastedImage_1.png

but also understand what this function is for doing.

pastedImage_4.png

I don't know why need to connects ch29.colud you tell me?

Thanks in advance.

タグ(3)
2 返答(返信)

1,943件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

if I understand this example correctly - in adcResultInMv_Vrefsh you get voltage reference high - which is connected to Channel 29. You don't need read this value - it is kind of feature for this example (you can setup breakpoint and check measured Voltage reference) - but not used for LEDs control. 

Hope it helps. 

Jiri

1,943件の閲覧回数
kemingkai
Contributor III

OK,I understand it.Thank you for your help, because there is no comment, I don’t dare to judge this function by experience.

0 件の賞賛
返信