The S32 Debugger included within the S32 Design Studio for S32 Platform IDE provides the ability to access the flash programming and debugging of the S32 Debug Probe via GDB command line. This document provides only the necessary commands specific to launching a debug session on NXP devices. It does not cover general GDB command line operations, these are covered in detail in the GNU communities and other public websites which are not associated with NXP.
Preparation
- Setup the software tools
- Install S32 Design Studio for S32 Platform
- Install the Development Package for the device you are debugging. In this case, the S32R41 development package. This package is important as the S32 Debugger support component contains the device-specific Python scripts required for initialization of the cores.
s32r41.PNG
- Setup the hardware
- Confirm the setup of the S32R41 evaluation board.
- Connect the power supply cable
- Setup the S32 Debug Probe. Refer to the S32 Debug Probe User Manual for installation instructions.
- Connect the S32 Debug Probe to the evaluation board via JTAG cable.
- Connect the S32 Debug Probe to the host PC via USB OR via Ethernet (via LAN or directly connected, and configured for static IP address) and power supply connected to USB port.
- Launch S32 Design Studio for S32 Platform
- Create new or open existing project and check that it successfully builds. If creating a new project, be sure the S32 Debugger is selected in the New Project Wizard

DanielBarbu_0-1718791409475.png
Procedure
As separate debug threads need to be started for each core to be debugged, and the method for launching a debug thread differs depending upon whether it is a primary core or secondary core and if the executable image will be loaded or if the executable is already running and the debugger just needs to be attached. These scenarios will be covered by the following 3 sections:
Primary Core Load Image and Run: The application image will be loaded directly to memory by the debugger and then initialized and started. The primary core will launch any secondary cores used by the application.
Secondary Cores: The primary core has launched a secondary core, it is now running and the debugger will connect through the attach method.
Primary Core Image Already In Memory and Running: The primary core has already been initialized and launched by other means, such as via a Linux OS on the target, so the debugger will connect through the attach method without initializing or loading the image to memory.
Please proceed with the section which applies to the core for which you are starting a debug thread.
Primary Core Load Image and Run
- Prepare the initialization script for the core(s) to be debugged.
- Open the core initialization Python script:
{S32DS Install Path}\S32DS\tools\S32Debugger\Debugger\scripts\s32r41\s32r41_generic_bareboard_all_cores.py

- Uncomment the following lines:
# _JTAG_SPEED = 16000
# _GDB_SERVER_PORT = 45000# _RESET_TYPE = "default"
# _PROBE_IP = "s32dbg"
# _CORE_NAME = 'M7_0'
# _RESET_DELAY = 1
# _REMOTE_TIMEOUT = 110
# _IS_LOGGING_ENABLED = False
# _SOC_NAME = "S32R41"
This file is used by the S32 Debugger within the S32 Design Studio IDE where the settings are provided from the GUI, so these lines are commented out in order to allow the GUI settings to have control. The commented lines are provided so the script could more easily be run by the command line method.
- Update the IP address line (_PROBE_IP) to match the IP address of the S32 Debug Probe which is connected to your PC. See the user guide for the S32 Debug Probe for details on how to obtain the IP address.
- Update the core name (_CORE_NAME), if necessary. See s32r41_context.py for complete list of supported cores.
- Save the file with a new name to preserve the original. For example, s32r41_gen_bb_all_c_my_probe.py. This ensures the S32 Debugger will still function correctly.

- Launch GTA server. From command prompt or Windows File Explorer run the command:
{S32DS Install Path}\S32DS\tools\S32Debugger\Debugger\Server\gta\gta.exe

Should see a window appear like this:

- Ensure Environment Variable for Python is set. From command prompt, run the command:
set PYTHONPATH={S32DS Install Path}\S32DS\build_tools\msys32\mingw32\lib\python2.7;{S32DS Install Path}\S32DS\build_tools\msys32\mingw32\lib\python2.7\site-packages

- Start GDB. In a command window, run the command:
Windows OS:
{S32DS Install Path}\S32DS\tools\gdb-arm\arm32-eabi\bin\arm-none-eabi-gdb-py.exe (for arm32)
OR
{S32DS Install Path}\S32DS\tools\gdb-arm\arm64-eabi\bin\aarch64-none-elf-gdb-py.exe (for arm64)
Linux OS: arm-none-eabi-gdb-py
A (gdb) prompt should now be displayed in the command window:

- From (gdb) prompt, enter the following commands(in this order):
- source {S32DS Install Path}\\S32DS\\tools\\S32Debugger\\Debugger\\scripts\\s32r41\\s32r41_gen_bb_all_c_my_probe.py
This specifies the script for initialization.
- py board_init()
This initializes the board. It should only be called for the initial core. In a multicore debugging workflow, the debugger launch for additional cores would omit this step.
- py core_init()
This initializes the core specified in the initialization script in step 1.

- Now standard GDB commands may be used. For example, you may wish to load an ELF file:
- file {S32DS Workspace Path}\\New_S32R_Project_M7_0\\Debug_RAM\\New_S32R_Project_M7_0.elf
- load

Secondary Cores
After completing the launch of debug for the primary core, it is possible to perform multicore debug by launching GDB debugging on the secondary cores.
- Some additional steps will need to be performed from within the primary core GDB session, enter the following commands:
set *0x34100000 = 0x34200000
set *0x34100004 = 0x34100025
set *0x34100024 = 0xFFFEF7FF
b main
c

These lines prepare the environment for launching debugging on secondary cores. This will allow for multicore debugging in the case of separate ELF files for each core. These can be found in the Run Commands field of the Startup tab on the Debug Configuration for the primary core within S32 Design Studio IDE, of any multicore project created from the New Application Project Wizard. Note: If there is just one ELF file for all cores, then these 'set *0x... = 0x...' commands should be skipped.
In general, it will be correct to set the break-point at main, as shown, but this might need to be changed depending on when the secondary cores are started within the project.

- Prepare the initialization script for the secondary core to be debugged.
- Open the core initialization Python script:
{S32DS Install Path}\S32DS\tools\S32Debugger\Debugger\scripts\s32r41\s32r41_attach.py
This is a different script than the one used for the primary core. It is designed to launch a debug session on a core which is already initialized and running.
- Edit the script for the secondary core to be debugged. Since this script is setup for the primary core, some adjustments need to be made to setup for a secondary core
- Uncomment the following lines:
# _JTAG_SPEED = 16000
# _GDB_SERVER_PORT = 45000
# _RESET_TYPE = "default"
# _PROBE_IP = "s32dbg"
# _CORE_NAME = 'M7_0'
# _RESET_DELAY = 1
# _REMOTE_TIMEOUT = 110
# _IS_LOGGING_ENABLED = False
# _SOC_NAME = "S32R41"
-
Make the following changes to the lines:
_JTAG_SPEED = 16000 -> None
_GDB_SERVER_PORT = 45000
_RESET_TYPE = "default"
_PROBE_IP = "s32dbg" -> None
_CORE_NAME = 'M7_0' -> 'M7_1' (this should be set to match the name of the core to be debugged, see s32r41_context.py for complete list)
_RESET_DELAY = 1
_REMOTE_TIMEOUT = 110
_IS_LOGGING_ENABLED = False -> ‘True’
_SOC_NAME = "S32R41"
- Save the file with a new name to preserve the original. For example, s32r41_attach_my_probe_core1.py. This ensures the S32 Debugger will still function correctly.

- The existing GTA server is used, so do not launch a new one.
- Open an new command window and follow similar steps as done for the primary core.
- Setup the Python environment variable, if not done globally
set PYTHONPATH={S32DS Install Path}\S32DS\build_tools\msys32\mingw32\lib\python2.7;{S32DS Install Path}\S32DS\build_tools\msys32\mingw32\lib\python2.7\site-packages
- Start GDB
Windows OS: {S32DS Install Path}\S32DS\tools\gdb-arm\arm32-eabi\bin\arm-none-eabi-gdb-py.exe (for arm32)
OR
{S32DS Install Path}\S32DS\tools\gdb-arm\arm64-eabi\bin\aarch64-none-elf-gdb-py.exe (for arm64)
Linux OS: arm-none-eabi-gdb-py
A (gdb) prompt should now be displayed in the command window:

- From (gdb) prompt, enter the following commands (in this order):
- source {S32DS Install Path}\\S32DS\\tools\\S32Debugger\\Debugger\\scripts\\s32r41\\s32r41_attach_my_probe_core1.py
This specifies the script for initialization.
- We will not execute the py board_init() as this was already done for the primary core.
- py core_init()
This initializes the core specified in the initialization script in step 2.

- Now standard GDB commands may be used. For example, you may wish to load an ELF file:
- file {S32DS Workspace Path}\\S32R_Multicore\\S32R_Multicore_M7_1\ \Debug_RAM\\S32R_Multicore_M7_1.elf
- load

Primary Core Image Already in Memory and Running
The core is running and does not need to be initialized.
- Prepare the initialization script for the core to be debugged.
- Open the core initialization Python script:
{S32DS Install Path}\S32DS\tools\S32Debugger\Debugger\scripts\s32r41\s32r41_attach.py
This is a different script than the one used for the primary core. It is designed to launch a debug session on a core which is already initialized and running.
- Edit the script for the secondary core to be debugged. Since this script is setup for the primary core, some adjustments need to be made to setup for a secondary core
- Uncomment the following lines:
# _JTAG_SPEED = 16000
# _GDB_SERVER_PORT = 45000
# _RESET_TYPE = "default"
# _PROBE_IP = "s32dbg"
# _CORE_NAME = 'M7_0'
# _RESET_DELAY = 1
# _REMOTE_TIMEOUT = 110
# _IS_LOGGING_ENABLED = False
# _SOC_NAME = "S32R41"
- Make the following changes to the lines:
_JTAG_SPEED = 16000
_GDB_SERVER_PORT = 45000
_RESET_TYPE = "default"
_PROBE_IP = "s32dbg" -> (enter the IP address of your probe)
_CORE_NAME = 'M7_0' (this should be set to match the name of the core to be debugged, see s32r41_context.py for complete list)
_RESET_DELAY = 1
_REMOTE_TIMEOUT = 110
_IS_LOGGING_ENABLED = False -> ‘True’
_SOC_NAME = "S32R41"
- Save the file with a new name to preserve the original. For example, s32r41_attach_my_probe_core0.py. This ensures the S32 Debugger will still function correctly.

- Launch GTA server. From command prompt or Windows File Explorer run the command:
{S32DS Install Path}\S32DS\tools\S32Debugger\Debugger\Server\gta\gta.exe

Should see a window appear like this:

- Ensure Environment Variable for Python is set. From command prompt, run the command:
set PYTHONPATH={S32DS Install Path}\S32DS\build_tools\msys32\mingw32\lib\python2.7;{S32DS Install Path}\S32DS\build_tools\msys32\mingw32\lib\python2.7\site-packages

- Start GDB. In a command window, run the command:
Windows OS:
{S32DS Install Path}\S32DS\tools\gdb-arm\arm32-eabi\bin\arm-none-eabi-gdb-py.exe (for arm32)
OR
{S32DS Install Path}\S32DS\tools\gdb-arm\arm64-eabi\bin\aarch64-none-elf-gdb-py.exe (for arm64)
Linux OS: arm-none-eabi-gdb-py
A (gdb) prompt should now be displayed in the command window:

- From (gdb) prompt, enter the following commands(in this order):
- source {S32DS Install Path}\\S32DS\\tools\\S32Debugger\\Debugger\\scripts\\s32r41\\s32r41_attach_my_probe_core0.py
This specifies the script for debugger initialization.
- Do not execute the py board_init() as this will initialize the board, and reset the currently executing application, which is not desired for this case.
- py core_init()
This initializes the debugger connection to the core specified in the initialization script in step 1.

- Now standard GDB commands may be used. For example, you may wish to load an ELF file:
- file {S32DS Workspace Path}\\ New_S32R41_Project\\New_S32R41_Project_M7_0\\Debug_RAM\\New_S32R41_Project_M7_0.elf
- load

- After completing the launch of debug for the primary core, it is possible to perform multicore debug by launching GDB debugging on the secondary cores. See section ‘Secondary Cores’ for each additional core to be debugged.