using interrupts with HCS12X

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

using interrupts with HCS12X

2,734 Views
RChapman
Contributor I
This message contains an entire topic ported from a separate forum. The original message and all replies are in this single message. We have seeded this new forum with selected information that we expect will be of value to you as you search for answers to your questions.
 
Posted: Mon Jul 25, 2005 6:55 am    
 
Hi! I'va another basic problem. How can I define an Interrupt with the microtimer or normal timer (vector from Xgate or HCS12?) and calling an Interrupt Sub Routine in C-language? Thank you very much for your help.
 
Posted: Fri Jul 29, 2005 8:18 pm    
 
are you using CodeWarrior?
 
Posted: Mon Aug 01, 2005 2:19 pm    
 
Yes I'm using CodeWarrior! I've solved the problem yet!! Someone sent me a working code example. If somebody is interested, I can send him a simple CodeWarrior project containing a RealTimerInterrupt-LED-toggle-on/off programm.
 
Posted: Mon Aug 01, 2005 7:07 pm    
 
You could post the code in the download area
 
Posted: Wed Aug 03, 2005 7:52 am    
 
I posted two small programms to the os cookbook for HCS12X processors.
On for the RTI and another one for Xgate.
If you have some ideas to improve this two programms you can send me an email. I'm a beginner with freescale MCU so I'll be happy if someone has nice ideas concerning this programms.
Labels (1)
0 Kudos
Reply
0 Replies