unsigned 64 bit integer not available

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

unsigned 64 bit integer not available

1,566 次查看
deneb
Contributor II

Hello

 

I am trying to use unsigned 64bit integer on an HCS12, as e.g.,

 

unsigned long long var1

 

But it turns out that it is always allocated as 32 bit unsigned. Upon checking the "Type Sizes" in the compiler options, I see that "long long" is declared as 32-bits. I cannot change it to 64-bits because that column is disabled.

Any ideas on how to overcome this issue?

 

Thanks

deneb

标签 (1)
0 项奖励
回复
1 回复

823 次查看
kef
Specialist I

You could do your own 64bit integer routines. These should be available on the net.

 

If execution time isn't issue and 52bits (0..+-2^52) are enough, then just use double instead of long long. Result of *-+/ should be the same, except that int/int may introduce fractional part and different behaviour on overflows.

 

Request imrpovement.

0 项奖励
回复