timer overflow interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

timer overflow interrupt

2,140 Views
zixia
Contributor II

The MCU I'm using is MC9S12P128,I want to use the overflow interrupt to record the number of overflows of the tcnt, but after I add the overflow interrupt, the program keeps going into the overflow interrupt. What's the problem?my timer prescaler value is TSCR2_PR=5, Timer clock = BUS_FREQ/(2^PREESCALER_VALUE) = 20MHz/32 = 625kHz; timer period = 1.6us。 My capture pulse cycle is 172ms, which means it will overflow once. The actual overflow interrupt in and out frequency is 4.2us. The interruption procedure is as follows: void interrupt TimerOverflow_Isr(void) { if(TFLG2_TOF == 1){ TFLG2 = 0x80; //CLEAR TOF PORTB_PB6 ^= 1; //TEST u16timeroverflow_Count++; } } Interrupt vector: TimerOverflow_Isr, /* 0x6F 0xFFDE ivVtimovf

0 Kudos
Reply
2 Replies

2,125 Views
zixia
Contributor II

Captures whether an interrupt conflicts with an overflow interrupt?

0 Kudos
Reply

2,082 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

 

 

There is not enough info in your description to say exactly what wrong you are doing. So, allow me to make considerations about your issue.

 

Just check….

The test for TOF is useless because interrupt means the TOF is set.

 

Tov = 65536 * (32/20,000,000) = 0.1048576 s … Timer period to overflow

Expected number of overflows 0.172s / 0.1048576 s = 1.64

 

Note: TFFCA

Timer Fast Flag Clear All

0 Allows the timer flag clearing to function normally.

1 For TFLG1(0x000E), a read from an input capture or a write to the output compare channel (0x0010–0x001F)

causes the corresponding channel flag, CnF, to be cleared. For TFLG2 (0x000F), any access to the TCNT

register (0x0004, 0x0005) clears the TOF flag. Any access to the PACNT registers (0x0022, 0x0023) clears

the PAOVF and PAIF flags in the PAFLG register (0x0021). This has the advantage of eliminating software

overhead in a separate clear sequence. Extra care is required to avoid accidental flag clearing due to

unintended accesses.

 

Moreover, bear in mind Write to TCNT has no meaning or effect in the normal mode; only writable in special modes. If you want to reset the TCNT for another period then it is necessary to combine it with “reset TCNT on TC7 overflow”.

 

Let’s suppose we will not use TFFCA. If we use it then interrupt flags are cleared manually. Do not combine TFFCA with manual clearing of flags.

 

Here I write the simple code, not tested, you can compare with yours.

Moreover think about other interrupts whether they are not so often that TOV is not executed because of its priority. Moreover, I think you check the TOV in debug mode and you forget to freeze timer in this mode... look in the code setup of TSCR1.

 

----------------------------------------------------

#pragma CODE_SEG NON_BANKED

interrupt 16 void TIM_Ovf_Isr(void);   // or interrupt ((0xFE-0xDE)/2) void TIM_TC7isr(void);

#pragma CODE_SEG DEFAULT

----------------------------------------------------

static unsigned long TIM_Ovf_Cnt=0;

----------------------------------------------------

#pragma CODE_SEG NON_BANKED

interrupt 16 void TIM_Ovf_Isr(void)    // or interrupt ((0xFE-0xDE)/2) void TIM_TC7isr(void);

{

  TFLG2 = 0x80;

  TIM_Ovf_Cnt++;

}

#pragma CODE_SEG DEFAULT

----------------------------------------------------

void main void

{

  //-------------------------------------

  // BUSCLK is 20MHz

  //.....................................

  //You know that you have this clock…

  //BUSCLK setup

 

  //-------------------------------------

  //Timer clock = BUS_FREQ/(2^PREESCALER_VALUE) = 20MHz/32 = 625kHz; timer period = 1.6us

  //.....................................

  TSCR2 = 0B10000101; // enable TIM ovf, No TIM reset dependance of the TC7 channel, PRSC = 32[d]

  TSCR1 = 0B11100000;// enab. tim, freeze tim in DBG mode and wait mode, no precision TIM, no fast flag clear

 

  //-------------------------------------

  // Enable I-bit maskable interrupts

  //.....................................

  ASM CLI;

 

  //-------------------------------------

  // main loop

  //.....................................

  while(1)

   {

    

   }

  //.....................................

 

}

 

 

Best regards,

Ladislav

0 Kudos
Reply