some Question about the function "adc" when i use s12zvml128 control pmsm foc (MC9S12ZVML128_PMSM_)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

some Question about the function "adc" when i use s12zvml128 control pmsm foc (MC9S12ZVML128_PMSM_)

Jump to solution
2,476 Views
Clarkhe
Contributor I

Hi

I use the single resistance sampling mode without a reference voltage of 2.5V. At present, I can only sample the current in one direction. Can I use the current demo simply to modify it? What is the efficiency?

Is there any problem. In addition, when the single resistance bus sampling will appear negative current?

0 Kudos
Reply
1 Solution
2,447 Views
pachamatej
NXP Employee
NXP Employee

Hi,

I'm just assuming, so if I'm not correct, please clarify.

In case you are using our devkits

https://www.nxp.com/design/development-boards/automotive-motor-control-solutions/magniv-and-s12-solu...

https://www.nxp.com/design/development-boards/automotive-motor-control-solutions/magniv-and-s12-solu...

https://www.nxp.com/design/development-boards/automotive-motor-control-solutions/magniv-and-s12-solu...

All three boards are capable of using DC-link shunt resistor to control a 3-ph motor, but the last two can do only this technique (aka "single-shunt" only).

If you are using the MTRCKTSPNZVM128 or MTRCKTSBNZVM128 (physically, it is the same devkit), then I would recommend to verify the jumper settings first according to the Quick start guide and the dedicated application note - there is a different configuration for dual-shunt and for single-shunt.

By the way, in all the cases, the reference voltage is 2.5V and thanks to that, the ADC can see positive and negative currents.

If you see any difference from what you want to achieve and from the description above, please let us know.

Best regards.

Matej

View solution in original post

0 Kudos
Reply
3 Replies
2,448 Views
pachamatej
NXP Employee
NXP Employee

Hi,

I'm just assuming, so if I'm not correct, please clarify.

In case you are using our devkits

https://www.nxp.com/design/development-boards/automotive-motor-control-solutions/magniv-and-s12-solu...

https://www.nxp.com/design/development-boards/automotive-motor-control-solutions/magniv-and-s12-solu...

https://www.nxp.com/design/development-boards/automotive-motor-control-solutions/magniv-and-s12-solu...

All three boards are capable of using DC-link shunt resistor to control a 3-ph motor, but the last two can do only this technique (aka "single-shunt" only).

If you are using the MTRCKTSPNZVM128 or MTRCKTSBNZVM128 (physically, it is the same devkit), then I would recommend to verify the jumper settings first according to the Quick start guide and the dedicated application note - there is a different configuration for dual-shunt and for single-shunt.

By the way, in all the cases, the reference voltage is 2.5V and thanks to that, the ADC can see positive and negative currents.

If you see any difference from what you want to achieve and from the description above, please let us know.

Best regards.

Matej

0 Kudos
Reply
2,430 Views
Clarkhe
Contributor I

OK,thankyou 

0 Kudos
Reply
2,460 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

I'm not sure if I understand.

Can you please elaborate?

 

Thank you,

BR, Daniel

 

0 Kudos
Reply