server web MC9S12NE64

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

server web MC9S12NE64

2,585件の閲覧回数
juanshaka
Contributor I
hello
 
i from colombia
 
i have the evaluation version of codewarrior HCS12 to MC9S12NE64 but it doesn't support the opentcp to be able to create a web server because opentcp have 72 file, somebody could help with an opentcp for the evaluation version it is that I need to send a series of data for ethernet, and I don't have a lot of idea of as making it.
 
however I had another idea and it was of making the web server with the help of the CMX-micronet but he/she has the problem that the tutorial that exists is for the full version and it doesn't stop evaluation version.
 
if somebody can help me with some of the files (opentcp or CMX-micronet) to carry out a web server for evaluation version.
 
please upload in the answer
 
PDT: i need the web server to my thesis
0 件の賞賛
返信
2 返答(返信)

1,453件の閲覧回数
mjbcswitzerland
Specialist V
Hi Juan

Take a look at the uTasker project. It will work with CW, IAR or GNU (the GNU compiler is free and has no file count restrictions). It also consists of an NE64 simulator which makes developing with it much easier and more efficient.

The uTasker is free for educational work and is fully supported (see its forum at www.uTasker.com/forum/).

The uTasker project includes all that you will need (HTTP, UART, FTP, TELNET, DHCP, etc.).

Regards

Mark

www.uTasker.com

0 件の賞賛
返信

1,453件の閲覧回数
juanshaka
Contributor I
ok  mjbcswitzerland
 
I will try to use it..... any doubt that I have will go by the forum
0 件の賞賛
返信