resolver connection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

resolver connection

2,873 Views
bezzie
Contributor I

hi,

   i am trying to connect resolver with MCSXSR1CS12ZVM evaluation board. is there inbuild excitation circuit for resolver. can i test resolver output on DSO by just connecting on evaluation board or  need to do some code for it. is there any example code available to get resolver position.

https://www.nxp.com/document/guide/get-started-with-the-mcsxsr1cs12zvm-evaluation-board-for-3-phase-...

0 Kudos
Reply
4 Replies

2,164 Views
jchabu
Contributor I

I am interested in the NXP software resolver. How could you claim that it is rated ASIL D(D) when safety mechanisms defined are related to only one sensor. For example, if the resolver measures 30 degrees (amplitude range, non-stuck signal, DC shift, zero-crossing, unit circle checks are correct) when the exact value is 40 degrees. How can you detect that? 

0 Kudos
Reply

2,702 Views
ImranAviconn
Contributor II

can you please provide the software example for resolver based feedback control for the MCSXSR1CS12ZVM evaluation board

0 Kudos
Reply

2,787 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

See attached

Best regards,

Ladislav

 

0 Kudos
Reply

2,687 Views
ImranAviconn
Contributor II

Hi,

Can you please share any example code for resolver feedback based control using the MCSXSR1CS127ZVM evaluation board

0 Kudos
Reply