programming rtc ds1307

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

programming rtc ds1307

2,830件の閲覧回数
emb
Contributor I
hi.
i need program for rtc ds1307 with  9s12xdt512 over I2C.
if anyone has,please send it to [email protected]
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,668件の閲覧回数
mke_et
Contributor IV
Well, first question would be do you want help with setting up the 12 to talk I2C to the clock chip? Or do you want help in how to talk to the RTC itself? I've interfaced it but I used the I2C pins as port pins and didn't use the I2C 'hardware'. I wrote my own routines since the part used for the project didn't have I2C support.

And I suppose it also matters if you are just looking for a template to paste in to your code?

Mike
0 件の賞賛
返信

1,668件の閲覧回数
emb
Contributor I
dear mike
           please send me the code that u had used to interface the RTC DS1307
           
0 件の賞賛
返信