programming rtc ds1307

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

programming rtc ds1307

2,845 Views
emb
Contributor I
hi.
i need program for rtc ds1307 with  9s12xdt512 over I2C.
if anyone has,please send it to [email protected]
Labels (1)
0 Kudos
Reply
2 Replies

1,683 Views
mke_et
Contributor IV
Well, first question would be do you want help with setting up the 12 to talk I2C to the clock chip? Or do you want help in how to talk to the RTC itself? I've interfaced it but I used the I2C pins as port pins and didn't use the I2C 'hardware'. I wrote my own routines since the part used for the project didn't have I2C support.

And I suppose it also matters if you are just looking for a template to paste in to your code?

Mike
0 Kudos
Reply

1,683 Views
emb
Contributor I
dear mike
           please send me the code that u had used to interface the RTC DS1307
           
0 Kudos
Reply