problem of 9s12dp512 memory map?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

problem of 9s12dp512 memory map?

2,187 次查看
jeffzxg
Contributor I
hi all
    dp512 has the following on chip resource:  1K register; 4K eeprom; 14K ram; 512K flash; where two 16K unpaged flash is located at $4000 ~ $7fff and $c000 ~ $ffff. and the reset address space for register is $0000 ~ $03ff ; eeprom is $0000 ~ $0fff ; ram $0800 ~ $3fff. priority is register > ram > eeprom > flash.
    so after reset the available space for register is 1K($0000~$3ff) ; ram 14K ($800 ~ $3fff) ; eeprom 1K ($400 ~ $7ff), but i want to fully use of 4K eeprom and 14K ram , so i have to remap the memory map of eeprom and ram space.
    ram space  extended to  next 16K address space ($4000 ~ $7fff) , according to the priority of on chip resource, the unpaged flash block ( $4000 ~ $7fff ) is overlapped.
    my question is: if  the unpaged flash block ( $4000 ~ $7fff ) is overlapped, does that mean i can not place any application code to that area? if it is right, is there any method that can use the overlapped flash areas?
                                           thanks!
标签 (1)
0 项奖励
回复
1 回复

1,117 次查看
kef
Specialist I
If you overlap part of unpaged 4000-7fff flash by RAM or EEPROM, then this overlapped flash is not accessible as unpaged flash, but it can be accessed as paged flash on PPAGE 3E.
 
I would move not 14k RAM but 4k EEPROM to 4000-4FFF. It would cover less of valuable unpaged flash. Unpaged flash is effective place to store const strings and const data. Accessing data from paged flash is cumbersome on S12.
0 项奖励
回复