prm file to extend RAM memory

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

prm file to extend RAM memory

Jump to solution
6,016 Views
freescale_satya
Contributor III
Hi, This is the sample PRM file i am using. I want to extend my RAM area for that i have made a change in PRM file in the following line from /* non-paged RAM */ RAM = READ_WRITE 0x2000 TO 0x3FFF ALIGN 2[1:1]; /* word align for XGATE accesses */ to /* non-paged RAM */ RAM = READ_WRITE 0x1000 TO 0x3FFF ALIGN 2[1:1]; /* word align for XGATE accesses */ but as soon as i run the program i get the COP watchdog timeout interrupt. could somebody help me on this? Iam new to PRM files. thanks in advance, regards, Satya
Labels (1)
0 Kudos
Reply
1 Solution
5,055 Views
freescale_satya
Contributor III
Hi Kef, Luckily i was able to resolve the issue. There was PAGED_RAM placement where i placed some of my variables by using #pragma directive and able to resolve the issue. Thanks for the support. Thanks again, Regards, Satya

View solution in original post

0 Kudos
Reply
6 Replies
5,055 Views
freescale_satya
Contributor III
sorry i failed to add the attachment.
0 Kudos
Reply
5,055 Views
freescale_satya
Contributor III
sorry it is not accepting attachments. i will paste it here ------------------- /* This is a linker parameter file for the MC9S12XEQ512 */ /* This parameter file is setup in a generic way to allow exploring most common features of both cores: - S12X core - XGATE code and constants in FLASH and/or RAM - XGATE data and stack in RAM It might be required to adapt some of the definitions to best match your application. */ NAMES /* CodeWarrior will pass all the needed files to the linker by command line. But here you may add your additional files */ END SEGMENTS /* here all RAM/ROM areas of the device are listed. Used in PLACEMENT below. All addresses are 'logical' */ /* Register space */ /* IO_SEG = PAGED 0x0000 TO 0x07FF; intentionally not defined */ /* non-paged EEPROM */ EEPROM = READ_ONLY 0x0C00 TO 0x0FFF; /* non-paged RAM */ RAM = READ_WRITE 0x2000 TO 0x3FFF ALIGN 2[1:1]; /* word align for XGATE accesses */ /* non-banked FLASH */ ROM_4000 = READ_ONLY 0x4000 TO 0x4FFF; ROM_C000 = READ_ONLY 0xC000 TO 0xFEFF; /* VECTORS = READ_ONLY 0xFF00 TO 0xFFFF; intentionally not defined: used for VECTOR commands below */ //OSVECTORS = READ_ONLY 0xFF10 TO 0xFFFF; /* OSEK interrupt vectors (use your vector.o) */ /* paged EEPROM 0x0800 TO 0x0BFF; addressed through EPAGE */ EEPROM_00 = READ_ONLY 0x000800 TO 0x000BFF; EEPROM_01 = READ_ONLY 0x010800 TO 0x010BFF; EEPROM_02 = READ_ONLY 0x020800 TO 0x020BFF; EEPROM_03 = READ_ONLY 0x030800 TO 0x030BFF; EEPROM_04 = READ_ONLY 0x040800 TO 0x040BFF; EEPROM_05 = READ_ONLY 0x050800 TO 0x050BFF; EEPROM_06 = READ_ONLY 0x060800 TO 0x060BFF; EEPROM_07 = READ_ONLY 0x070800 TO 0x070BFF; EEPROM_08 = READ_ONLY 0x080800 TO 0x080BFF; EEPROM_09 = READ_ONLY 0x090800 TO 0x090BFF; EEPROM_0A = READ_ONLY 0x0A0800 TO 0x0A0BFF; EEPROM_0B = READ_ONLY 0x0B0800 TO 0x0B0BFF; EEPROM_0C = READ_ONLY 0x0C0800 TO 0x0C0BFF; EEPROM_0D = READ_ONLY 0x0D0800 TO 0x0D0BFF; EEPROM_0E = READ_ONLY 0x0E0800 TO 0x0E0BFF; EEPROM_0F = READ_ONLY 0x0F0800 TO 0x0F0BFF; EEPROM_10 = READ_ONLY 0x100800 TO 0x100BFF; EEPROM_11 = READ_ONLY 0x110800 TO 0x110BFF; EEPROM_12 = READ_ONLY 0x120800 TO 0x120BFF; EEPROM_13 = READ_ONLY 0x130800 TO 0x130BFF; EEPROM_14 = READ_ONLY 0x140800 TO 0x140BFF; EEPROM_15 = READ_ONLY 0x150800 TO 0x150BFF; EEPROM_16 = READ_ONLY 0x160800 TO 0x160BFF; EEPROM_17 = READ_ONLY 0x170800 TO 0x170BFF; EEPROM_18 = READ_ONLY 0x180800 TO 0x180BFF; EEPROM_19 = READ_ONLY 0x190800 TO 0x190BFF; EEPROM_1A = READ_ONLY 0x1A0800 TO 0x1A0BFF; EEPROM_1B = READ_ONLY 0x1B0800 TO 0x1B0BFF; EEPROM_1C = READ_ONLY 0x1C0800 TO 0x1C0BFF; EEPROM_1D = READ_ONLY 0x1D0800 TO 0x1D0BFF; EEPROM_1E = READ_ONLY 0x1E0800 TO 0x1E0BFF; EEPROM_1F = READ_ONLY 0x1F0800 TO 0x1F0BFF; EEPROM_FC = READ_ONLY 0xFC0800 TO 0xFC0BFF; EEPROM_FD = READ_ONLY 0xFD0800 TO 0xFD0BFF; EEPROM_FE = READ_ONLY 0xFE0800 TO 0xFE0BFF; /* EEPROM_FF = READ_ONLY 0xFF0800 TO 0xFF0BFF; intentionally not defined: equivalent to EEPROM */ /* paged RAM: 0x1000 TO 0x1FFF; addressed through RPAGE */ RAM_XGATE_STK_L_ = NO_INIT 0xF81000 TO 0xF8107D; RAM_XGATE_STK_L = NO_INIT 0xF8107E TO 0xF8107F; RAM_XGATE_STK_H_ = NO_INIT 0xF81080 TO 0xF810FD; RAM_XGATE_STK_H = NO_INIT 0xF810FE TO 0xF810FF; RAM_F8 = READ_WRITE 0xF81100 TO 0xF81FFF ALIGN 2[1:1]; /* is also mapped to XGATE: 0x8100..0x8FFF */ RAM_F9 = READ_WRITE 0xF91000 TO 0xF91FFF ALIGN 2[1:1]; /* is also mapped to XGATE: 0x9000..0x9FFF */ RAM_FA = READ_WRITE 0xFA1000 TO 0xFA1FFF ALIGN 2[1:1]; /* is also mapped to XGATE: 0xA000..0xAFFF */ RAM_FB = READ_WRITE 0xFB1000 TO 0xFB1FFF ALIGN 2[1:1]; /* is also mapped to XGATE: 0xB000..0xBFFF */ RAM_FC = READ_WRITE 0xFC1000 TO 0xFC1FFF ALIGN 2[1:1]; /* is also mapped to XGATE: 0xC000..0xCFFF */ RAM_FD = READ_WRITE 0xFD1000 TO 0xFD1FFF ALIGN 2[1:1]; /* is also mapped to XGATE: 0xD000..0xDFFF */ /* RAM_FE = READ_WRITE 0xFE1000 TO 0xFE1FFF; intentionally not defined: equivalent to RAM: 0x2000..0x2FFF */ /* RAM_FF = READ_WRITE 0xFF1000 TO 0xFF1FFF; intentionally not defined: equivalent to RAM: 0x3000..0x3FFF */ /* paged FLASH: 0x8000 TO 0xBFFF; addressed through PPAGE */ PAGE_E0_0 = READ_ONLY 0xE08000 TO 0xE087FF; /* cannot be mapped to XGATE; XGATE sees registers here */ PAGE_E0 = READ_ONLY 0xE08800 TO 0xE0BFFF ALIGN 2[1:1]; /* is also mapped to XGATE: 0x0800..0x3FFF */ PAGE_E1 = READ_ONLY 0xE18000 TO 0xE1BFFF ALIGN 2[1:1]; /* is also mapped to XGATE: 0x4000..0x7FFF */ // cannot be mapped to XGATE; this module should NOT be used for HC12 code when also used for XGATE code since //the HC12 will have priority over the XGATE accessing the FLASH modules resulting very poor performance of //the XGATE: Check allocation of this ranges in PLACEMENT below! PAGE_E2 = READ_ONLY 0xE28000 TO 0xE2BFFF; PAGE_E3 = READ_ONLY 0xE38000 TO 0xE3BFFF; PAGE_E4 = READ_ONLY 0xE48000 TO 0xE4BFFF; PAGE_E5 = READ_ONLY 0xE58000 TO 0xE5BFFF; PAGE_E6 = READ_ONLY 0xE68000 TO 0xE6BFFF; PAGE_E7 = READ_ONLY 0xE78000 TO 0xE7BFFF; PAGE_E8 = READ_ONLY 0xE88000 TO 0xE8BFFF; PAGE_E9 = READ_ONLY 0xE98000 TO 0xE9BFFF; PAGE_EA = READ_ONLY 0xEA8000 TO 0xEABFFF; PAGE_EB = READ_ONLY 0xEB8000 TO 0xEBBFFF; PAGE_EC = READ_ONLY 0xEC8000 TO 0xECBFFF; PAGE_ED = READ_ONLY 0xED8000 TO 0xEDBFFF; PAGE_EE = READ_ONLY 0xEE8000 TO 0xEEBFFF; PAGE_EF = READ_ONLY 0xEF8000 TO 0xEFBFFF; PAGE_F0 = READ_ONLY 0xF08000 TO 0xF0BFFF; PAGE_F1 = READ_ONLY 0xF18000 TO 0xF1BFFF; PAGE_F2 = READ_ONLY 0xF28000 TO 0xF2BFFF; PAGE_F3 = READ_ONLY 0xF38000 TO 0xF3BFFF; PAGE_F4 = READ_ONLY 0xF48000 TO 0xF4BFFF; PAGE_F5 = READ_ONLY 0xF58000 TO 0xF5BFFF; PAGE_F6 = READ_ONLY 0xF68000 TO 0xF6BFFF; PAGE_F7 = READ_ONLY 0xF78000 TO 0xF7BFFF; PAGE_F8 = READ_ONLY 0xF88000 TO 0xF8BFFF; PAGE_F9 = READ_ONLY 0xF98000 TO 0xF9BFFF; PAGE_FA = READ_ONLY 0xFA8000 TO 0xFABFFF; PAGE_FB = READ_ONLY 0xFB8000 TO 0xFBBFFF; PAGE_FC = READ_ONLY 0xFC8000 TO 0xFCBFFF; /* PAGE_FD = READ_ONLY 0xFD8000 TO 0xFDBFFF; intentionally not defined: equivalent to ROM_4000 */ PAGE_FE = READ_ONLY 0xFE8000 TO 0xFEBFFF; /* PAGE_FF = READ_ONLY 0xFF8000 TO 0xFFBFFF; intentionally not defined: equivalent to ROM_C000 */ END PLACEMENT /* here all predefined and user segments are placed into the SEGMENTS defined above. */ _PRESTART, /* Used in HIWARE format: jump to _Startup at the code start */ STARTUP, /* startup data structures */ ROM_VAR, /* constant variables */ STRINGS, /* string literals */ VIRTUAL_TABLE_SEGMENT, /* C++ virtual table segment */ //.ostext, /* eventually OSEK code */ NON_BANKED, /* runtime routines which must not be banked */ COPY /* copy down information: how to initialize variables */ /* in case you want to use ROM_4000 here as well, make sure that all files (incl. library files) are compiled with the option: -OnB=b */ INTO ROM_C000/*, ROM_4000*/; DEFAULT_ROM INTO PAGE_FE, PAGE_FC, PAGE_FB, PAGE_FA, PAGE_F9, PAGE_F8, PAGE_F7, PAGE_F6, PAGE_F5, PAGE_F4, PAGE_F3, PAGE_F2, PAGE_F1, PAGE_F0, PAGE_EF, PAGE_EE, PAGE_ED, PAGE_EC, PAGE_EB, PAGE_EA, PAGE_E9, PAGE_E8, PAGE_E7, PAGE_E6, PAGE_E5, PAGE_E4, PAGE_E3, PAGE_E2, /* PAGE_E1 intentionally not listed: assigned to XGATE */ /* PAGE_E0 intentionally not listed: assigned to XGATE */ PAGE_E0_0; XGATE_VECTORS, /* XGATE vector table is allocated in FLASH */ XGATE_STRING, /* XGATE string literals */ XGATE_CONST, /* XGATE constants */ XGATE_CODE, /* XGATE functions */ XGATE_STRING_FLASH, /* XGATE strings that should always go into flash */ XGATE_CONST_FLASH, /* XGATE constants what should always go into flash */ XGATE_CODE_FLASH /* XGATE code that should always run out of flash */ INTO PAGE_E0, PAGE_E1; /* FLASH accessible by XGATE */ //.stackstart, /* eventually used for OSEK kernel awareness: Main-Stack Start */ SSTACK, /* allocate stack first to avoid overwriting variables on overflow */ //.stackend, /* eventually used for OSEK kernel awareness: Main-Stack End */ DEFAULT_RAM /* all variables, the default RAM location */ INTO RAM; SHARED_DATA /* variables that are shared between CPU12 and XGATE */ INTO RAM; XGATE_STRING_RAM, /* XGATE strings that should always go into RAM */ XGATE_CONST_RAM, /* XGATE constants what should always go into RAM */ XGATE_CODE_RAM, /* XGATE code that should always run out of RAM */ XGATE_DATA /* data that are accessed by XGATE only */ INTO RAM_F8, RAM_F9, RAM_FA, RAM_FB /*, RAM_FC, RAM_FD */; PAGED_RAM /* paged data accessed by CPU12 only */ INTO /* when using banked addressing for variable data, make sure to specify the option -D__FAR_DATA on the compiler command line */ RAM_FD, RAM_FC /*, RAM_FB, RAM_FA, RAM_F9 */; XGATE_STK_L INTO RAM_XGATE_STK_L; XGATE_STK_H INTO RAM_XGATE_STK_H; //.vectors INTO OSVECTORS; /* OSEK vector table */ END ENTRIES /* keep the following unreferenced variables */ /* OSEK: always allocate the vector table and all dependent objects */ //_vectab OsBuildNumber _OsOrtiStackStart _OsOrtiStart END STACKSIZE 0x200 /* size of the stack (will be allocated in DEFAULT_RAM) */ /* use these definitions in plane of the vector table ('vectors') above */ VECTOR 0 _Startup /* reset vector: this is the default entry point for a C/C++ application. */ //VECTOR 0 Entry /* reset vector: this is the default entry point for an Assembly application. */ //INIT Entry /* for assembly applications: that this is as well the initialization entry point */
0 Kudos
Reply
5,055 Views
kef
Specialist I

What you pasted is totally not readable.

 

You can extend nonbanked RAM to start from 0x1000. But then you should remove RAM_FC from banked RAM. Also you have to not use RPAGE for far RAM accesses. All far RAM segments should be made not __RPAGE_SEG, but __GPAGE_SEG.

You should determine yourself was COP triggered because code run away, or because you increased size of data and initialization or some other routine is now taking too long to execute.

0 Kudos
Reply
5,055 Views
freescale_satya
Contributor III
Hi Kef, I am facing some issues with the browser the edit box to enter the data is very small and unable to preview the data as well. i have to rectify this then only i can post any message. But the prm file i have taken is a standard prm file. i just changed ram starting to 0x1000 then immediately it resets. i have not written any seperate cop watchdog timeout i think it is part of start12.c file. As you told i made changes in the prm file but i do not know where to change what u have said _RPAGE_SEG and _GPAGE_SEG. But still once i make 0x1000 the cop reset happens. I donot know how to proceed. Please help me. thanks again Satya
0 Kudos
Reply
5,055 Views
kef
Specialist I

Did you enable COP? It should be disabled by default.

What memory model are you using? If "standard" banked model, then are you using far RAM at all? If not, then you can forget what I told you, __GPAGE_SEG, __RPAGE_SEG etc. In banked model by default all vvariables are near and it is quite safe then to edit RAM to 0x1000-0x3FFF. It should work without any problem.

More static storage RAM variables you have, more time it takes to zero them all at startup. Initializing variables with static initializer takes additional time. In case you are using some system management chip with COP always enabled, you may need to edit startup file to service COP duing zeroout.

 

0 Kudos
Reply
5,056 Views
freescale_satya
Contributor III
Hi Kef, Luckily i was able to resolve the issue. There was PAGED_RAM placement where i placed some of my variables by using #pragma directive and able to resolve the issue. Thanks for the support. Thanks again, Regards, Satya
0 Kudos
Reply