printf and RAM consumption issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

printf and RAM consumption issue

跳至解决方案
7,342 次查看
fqh
Contributor II

 

129 printf("%d %ld %u\n", 999, 9999, 99);
0xfe8a5b: 900063 LD D2,#99
0xfe8a5e: 0402 PSH D2
0xfe8a60: 90270F LD D2,#9999
0xfe8a63: 0402 PSH D2
0xfe8a65: 9003E7 LD D2,#999
0xfe8a68: 0402 PSH D2
0xfe8a6a: 98001217 LD X,#4631
0xfe8a6e: 0442 PSH X
0xfe8a70: BBFEF8F2 JSR 16709874 printf (0xfef8f2)
0xfe8a74: 0A69 LEA S,(9,S)

 

CodeWarrior for MCU
Version: 10.7
Build Id:160721

When compiled, the string "%d %ld %u\n" is located in flash. During startup, it will be copied from flash to RAM, so you can see a RAM address 4631 (0x1217) is set to X register. Is the copy operation required? If yes, there are many many printf functions in our code, they will consume many many RAM space.

 

标记 (1)
0 项奖励
回复
1 解答
7,200 次查看
stanish
NXP Employee
NXP Employee

Hi,

strings are considered as data by default.

To avoid copydown you can place pragma below:

 

#pragma readonly_strings on

 

e.g. add a prefix file (e.g. myPrefix.h):

 

#ifndef MYPREFIX_H_
#define MYPREFIX_H_

#pragma readonly_strings on

#endif /* MYPREFIX_H_ */

 

 to include it to every source file in your project you add the prefix file here:

stanish_0-1732654275311.png

Now the object that represents strings (@148 in my example)is located at flash:

stanish_0-1732654442485.png

 

 

Hope it helps,

Stan

 

 

在原帖中查看解决方案

7 回复数
5,217 次查看
Saundersa
Contributor I

I ran into the same concern on an embedded project using CodeWarrior (10.x) for an HCS12. Our fix was placing string literals in flash with a const qualifier and using a printf variant that reads from ROM, avoiding RAM copies. Otherwise, stack/RAM usage ballooned fast. If you can’t change printf, consider a tiny logger with format tokens. For stress-testing memory behavior, I oddly used Solar Smash as a playful metaphor app during breaks—it helped me think about “controlled destruction.”

0 项奖励
回复
7,293 次查看
RyanJohnson1
Contributor I

This code showcases a memory management process, illustrating how data is transferred from flash to RAM using printf. Interestingly, just like https://slope3dgame.com/ mastering the requires understanding optimal trajectories and resource allocation, effective memory handling ensures efficient performance in programming. The redundant copy operations could waste valuable RAM, just like time wasted in the game without sharp strategies.

7,311 次查看
lama
NXP TechSupport
NXP TechSupport

Hi,

everything depends on your variable definition.

If it is RAM variable then it will be copied to the RAM and used as a RAM variable.

If it is defined as a volatile constant and placed into EEPROM space or any rom or const segment then it will be used from this space. You can create your special space for text constants (or not) in the PRM file ( can be found in the Linker Files folder of your project ) and then use it for constants placement.

Best regards,

Ladislav

 

0 项奖励
回复
7,297 次查看
fqh
Contributor II

Hi,

You may not know what I mean.

The format string "%d %ld %u\n" should be a constant, and it has been placed in the flash. During the startup, I mean in the initialization, or to be exact, in the function DoCopyDown(), (in the startup code, file starts12z.c) this string content is copied to RAM again. In the disassembly window, we can see this string is copied to memory address 4631 (0x1217), so 4631 is loaded to X pointer register.

Why not pass the flash address of this format string to printf, why we need the copy operation?

0 项奖励
回复
7,284 次查看
lama
NXP TechSupport
NXP TechSupport

Hi,

it is not copy down function. I understood your issue wrong. It is just saving parameters onto stack for passing them to the function. It is standard parameters passing. Copy down function is a part of startup code - it is different story.

Of course, if you have repeating values and or strings you can create a set of outputs and send them all as a strings.

prm file>

* non-paged FLASHs */
ROM = READ_ONLY 0xFE0200 TO 0xFFFDFF;
ROM_STRINGS = READ_ONLY 0xFE0000 TO 0xFE01FF;

....

...

DEFAULT_RAM INTO RAM;

ROM_STRINGS INTO ROM_STRINGS;

....

 

main.c>

 

#pragma CONST_SEG ROM_STRINGS  // part of the ROM stolen from entire ROM in the PRM file

unsigned char const s1[]="string1";
unsigned char const s2[]="string2";
unsigned char const s3[]="string3";
unsigned char const s4[]="string4";
unsigned char const s5[]="string5";

#pragma CONST_SEG DEFAULT

//**************************************

void main(void)
{

for(;;)
{
  printf("s1 = %s\n", s1);

  printf("s1 = %s\n", s2); 

  printf("s1 = %s\n", s3); 

}
}

Best regard,

Ladislav

0 项奖励
回复
7,230 次查看
fqh
Contributor II

Hi,

It is copy down function. The evidences are listed below:

1. If we set a watchpoint at the RAM address (4631 (0x1217)), the program will stop there during DoCopyDown execution.

fqh_0-1732505193489.png

2. The string "%d %ld %u\n" is located at both RAM and flash:

fqh_1-1732505569730.pngfqh_2-1732505621548.png

3. The COPYDOWN section

fqh_3-1732505703360.png

 

0 项奖励
回复
7,201 次查看
stanish
NXP Employee
NXP Employee

Hi,

strings are considered as data by default.

To avoid copydown you can place pragma below:

 

#pragma readonly_strings on

 

e.g. add a prefix file (e.g. myPrefix.h):

 

#ifndef MYPREFIX_H_
#define MYPREFIX_H_

#pragma readonly_strings on

#endif /* MYPREFIX_H_ */

 

 to include it to every source file in your project you add the prefix file here:

stanish_0-1732654275311.png

Now the object that represents strings (@148 in my example)is located at flash:

stanish_0-1732654442485.png

 

 

Hope it helps,

Stan

 

 

%3CLINGO-SUB%20id%3D%22lingo-sub-1997035%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3Eprintf%20%E5%92%8C%20RAM%20%E6%B6%88%E8%80%97%E9%97%AE%E9%A2%98%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-1997035%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CBR%20%2F%3E%3CPRE%20class%3D%22lia-code-sample%20language-c%22%3E%3CCODE%20translate%3D%22no%22%3E129%20printf(%22%25d%20%25ld%20%25u%5Cn%22%2C%20999%2C%209999%2C%2099)%3B%0A0xfe8a5b%3A%20900063%20LD%20D2%2C%2399%0A0xfe8a5e%3A%200402%20PSH%20D2%0A0xfe8a60%3A%2090270F%20LD%20D2%2C%239999%0A0xfe8a63%3A%200402%20PSH%20D2%0A0xfe8a65%3A%209003E7%20LD%20D2%2C%23999%0A0xfe8a68%3A%200402%20PSH%20D2%0A0xfe8a6a%3A%2098001217%20LD%20X%2C%234631%0A0xfe8a6e%3A%200442%20PSH%20X%0A0xfe8a70%3A%20BBFEF8F2%20JSR%2016709874%20printf%20(0xfef8f2)%0A0xfe8a74%3A%200A69%20LEA%20S%2C(9%2CS)%3C%2FCODE%3E%3C%2FPRE%3E%3CBR%20%2F%3E%3CP%3EMCU%20%E7%9A%84%20CodeWarrior%3CBR%20%2F%3E%E7%89%88%E6%9C%AC%EF%BC%9A10.7%3CBR%20%2F%3E%E7%89%88%E6%9C%AC%E5%8F%B7%EF%BC%9A160721%3C%2FP%3E%3CP%3E%E7%BC%96%E8%AF%91%E5%90%8E%EF%BC%8C%E5%AD%97%E7%AC%A6%E4%B8%B2%E2%80%9C%EF%BC%85d%EF%BC%85ld%EF%BC%85u%20%5Cn%E2%80%9D%E4%BD%8D%E4%BA%8Eflash%E4%B8%AD%E3%80%82%E5%9C%A8%E5%90%AF%E5%8A%A8%E8%BF%87%E7%A8%8B%E4%B8%AD%EF%BC%8C%E5%AE%83%E5%B0%86%E4%BB%8E%E9%97%AA%E5%AD%98%E5%A4%8D%E5%88%B6%E5%88%B0%20RAM%EF%BC%8C%E5%9B%A0%E6%AD%A4%E6%82%A8%E5%8F%AF%E4%BB%A5%E7%9C%8B%E5%88%B0%20RAM%20%E5%9C%B0%E5%9D%80%204631%EF%BC%880x1217%EF%BC%89%E8%A2%AB%E8%AE%BE%E7%BD%AE%E4%B8%BA%20X%20%E5%AF%84%E5%AD%98%E5%99%A8%E3%80%82%E6%98%AF%E5%90%A6%E9%9C%80%E8%A6%81%E8%BF%9B%E8%A1%8C%E5%A4%8D%E5%88%B6%E6%93%8D%E4%BD%9C%EF%BC%9F%E5%A6%82%E6%9E%9C%E6%98%AF%E7%9A%84%E8%AF%9D%EF%BC%8C%E6%88%91%E4%BB%AC%E7%9A%84%E4%BB%A3%E7%A0%81%E4%B8%AD%E4%BC%9A%E6%9C%89%E5%BE%88%E5%A4%9Aprintf%E5%87%BD%E6%95%B0%EF%BC%8C%E5%AE%83%E4%BB%AC%E4%BC%9A%E6%B6%88%E8%80%97%E5%BE%88%E5%A4%9A%E5%BE%88%E5%A4%9A%E7%9A%84RAM%E7%A9%BA%E9%97%B4%E3%80%82%3C%2FP%3E%3CBR%20%2F%3E%3C%2FLINGO-BODY%3E%3CLINGO-SUB%20id%3D%22lingo-sub-1999573%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%E5%9B%9E%E5%A4%8D%EF%BC%9Aprintf%20%E5%92%8C%20RAM%20%E6%B6%88%E8%80%97%E9%97%AE%E9%A2%98%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-1999573%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3E%E6%AD%A4%E4%BB%A3%E7%A0%81%E5%B1%95%E7%A4%BA%E4%BA%86%E5%86%85%E5%AD%98%E7%AE%A1%E7%90%86%E8%BF%87%E7%A8%8B%EF%BC%8C%E8%AF%B4%E6%98%8E%E4%BA%86%E5%A6%82%E4%BD%95%E4%BD%BF%E7%94%A8%20printf%20%E5%B0%86%E6%95%B0%E6%8D%AE%E4%BB%8E%E9%97%AA%E5%AD%98%E4%BC%A0%E8%BE%93%E5%88%B0%20RAM%E3%80%82%E6%9C%89%E8%B6%A3%E7%9A%84%E6%98%AF%EF%BC%8C%E5%B0%B1%E5%83%8F%E6%8E%8C%E6%8F%A1%3CA%20href%3D%22https%3A%2F%2Fslope3dgame.com%2F%22%20target%3D%22_blank%22%20rel%3D%22nofollow%20noopener%20noreferrer%22%3Ehttps%3A%2F%2Fslope3dgame.com%2F%3C%2FA%3E%E9%9C%80%E8%A6%81%E4%BA%86%E8%A7%A3%E6%9C%80%E4%BD%B3%E8%BD%A8%E8%BF%B9%E5%92%8C%E8%B5%84%E6%BA%90%E5%88%86%E9%85%8D%E4%B8%80%E6%A0%B7%EF%BC%8C%E6%9C%89%E6%95%88%E7%9A%84%E5%86%85%E5%AD%98%E5%A4%84%E7%90%86%E5%8F%AF%E7%A1%AE%E4%BF%9D%E7%BC%96%E7%A8%8B%E7%9A%84%E9%AB%98%E6%95%88%E6%80%A7%E8%83%BD%E3%80%82%E5%86%97%E4%BD%99%E7%9A%84%E5%A4%8D%E5%88%B6%E6%93%8D%E4%BD%9C%E4%BC%9A%E6%B5%AA%E8%B4%B9%E5%AE%9D%E8%B4%B5%E7%9A%84RAM%EF%BC%8C%E5%B0%B1%E5%83%8F%E5%9C%A8%E6%B8%B8%E6%88%8F%E4%B8%AD%E6%B2%A1%E6%9C%89%E6%95%8F%E9%94%90%E7%9A%84%E7%AD%96%E7%95%A5%E8%80%8C%E6%B5%AA%E8%B4%B9%E6%97%B6%E9%97%B4%E4%B8%80%E6%A0%B7%E3%80%82%3C%2FP%3E%3C%2FLINGO-BODY%3E%3CLINGO-SUB%20id%3D%22lingo-sub-2169458%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%20translate%3D%22no%22%3ERe%3A%20printf%20and%20RAM%20consumption%20issue%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2169458%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3E%3CSPAN%3E%E6%88%91%E5%9C%A8%E4%B8%80%E4%B8%AA%E4%BD%BF%E7%94%A8%20CodeWarrior%20(10.x)%20%E7%9A%84%20HCS12%20%E5%B5%8C%E5%85%A5%E5%BC%8F%E9%A1%B9%E7%9B%AE%E4%B8%AD%E9%81%87%E5%88%B0%E4%BA%86%E5%90%8C%E6%A0%B7%E7%9A%84%E9%97%AE%E9%A2%98%E3%80%82%E6%88%91%E4%BB%AC%E7%9A%84%E8%A7%A3%E5%86%B3%E5%8A%9E%E6%B3%95%E6%98%AF%E5%B0%86%E5%AD%97%E7%AC%A6%E4%B8%B2%E5%AD%97%E9%9D%A2%E9%87%8F%E6%94%BE%E5%9C%A8%E9%97%AA%E5%AD%98%E4%B8%AD%EF%BC%8C%E5%B9%B6%E4%BD%BF%E7%94%A8%20const%20%E9%99%90%E5%AE%9A%E7%AC%A6%EF%BC%8C%E7%84%B6%E5%90%8E%E4%BD%BF%E7%94%A8%20printf%20%E5%8F%98%E4%BD%93%E4%BB%8E%20ROM%20%E8%AF%BB%E5%8F%96%EF%BC%8C%E9%81%BF%E5%85%8D%20RAM%20%E5%A4%8D%E5%88%B6%E3%80%82%E5%90%A6%E5%88%99%EF%BC%8C%E5%A0%86%E6%A0%88%2F%E5%86%85%E5%AD%98%E4%BD%BF%E7%94%A8%E9%87%8F%E4%BC%9A%E8%BF%85%E9%80%9F%E8%86%A8%E8%83%80%E3%80%82%E5%A6%82%E6%9E%9C%E6%97%A0%E6%B3%95%E6%9B%B4%E6%94%B9%20printf%EF%BC%8C%E5%8F%AF%E4%BB%A5%E8%80%83%E8%99%91%E4%BD%BF%E7%94%A8%E6%A0%BC%E5%BC%8F%E6%A0%87%E8%AE%B0%E7%9A%84%E5%BE%AE%E5%B0%8F%E6%97%A5%E5%BF%97%E8%AE%B0%E5%BD%95%E5%99%A8%E3%80%82%E4%B8%BA%E4%BA%86%E6%B5%8B%E8%AF%95%E8%AE%B0%E5%BF%86%E8%A1%8C%E4%B8%BA%E7%9A%84%E5%8E%8B%E5%8A%9B%EF%BC%8C%E6%88%91%E5%9C%A8%E4%BC%91%E6%81%AF%E6%97%B6%E5%A5%87%E6%80%AA%E5%9C%B0%E6%8A%8A%3CA%20href%3D%22https%3A%2F%2Fsolarsmashonline.com%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3ESolar%20Smash%3C%2FA%3E%E4%BD%9C%E4%B8%BA%E4%B8%80%E4%B8%AA%E6%9C%89%E8%B6%A3%E7%9A%84%E9%9A%90%E5%96%BB%E5%BA%94%E7%94%A8--%E5%AE%83%E5%B8%AE%E5%8A%A9%E6%88%91%E6%80%9D%E8%80%83%20%22%E6%9C%89%E6%8E%A7%E5%88%B6%E7%9A%84%E7%A0%B4%E5%9D%8F%22%E3%80%82%3C%2FSPAN%3E%3C%2FP%3E%3C%2FLINGO-BODY%3E