microcontroller problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

microcontroller problem

2,953 Views
hosseings
Contributor II

Hi every body. There is a MC9S12XHZ256 microcontroller in truck dashboard. a battery cable disconnect from alternator and the circuit was burned. now when i ohm test the micro, there is a short circuit between Vdd and Vss. what's the problem?

4 Replies

2,724 Views
dsherman
Contributor III

Most likely destroyed.  You did say the circuit burned.  Depending on what was disconnected the alternator may have railed to a high voltage and that's what killed it.

2,724 Views
hosseings
Contributor II

thanks David. i removed the micro from the board, but there is still a short circuit in the board. i disconnect all Vdd and Vss ics's pins from pcb but can't detect the short circuit.

0 Kudos
Reply

2,724 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Hossein, 

It could be a bulk/decoupling capacitor between VDD, VSS.

Regards,

Daniel

2,724 Views
hosseings
Contributor II

Thank you Daniel

0 Kudos
Reply