memory map for 9s12q128 for usbdm memory dump

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

memory map for 9s12q128 for usbdm memory dump

2,798 次查看
evkuchevkuch
Contributor I

Good day! I have (9s12q128), usbdm 4.12.1 and memory dump, Prompt please Referring I should specify the address for the correct reading of the chip so that later I could write a new chip? I have read datasheet, but still do not understand ..

Original Attachment has been moved to: usbdm--memory-dunp.rar

标签 (1)
0 项奖励
回复
2 回复数

2,290 次查看
lama
NXP TechSupport
NXP TechSupport

Ups, you are talkiung about Q128 (not G128).

In this case the memory spce you have to get is:

ppage 0x38-0x3F

offsett 8000-BFFF for each page

best regards,

Ladislav

0 项奖励
回复

2,290 次查看
lama
NXP TechSupport
NXP TechSupport

Hi,

it is not absolutely clear what you really have. If it is only copy of the memory and it contains entire memory then the address is given by memory map. Moreover, I do not know your programming mechanism but you should keep in mind that S12G uses global addresses for memory programming and PPAGE_offset addressing for memory reading. So your question opens more questions. As a start I would like to present you memory map of the device.

If you are not sure of data placement and you do not have S12 record (which is the best for programming) then the best way I see is to store entire memory including not programmed spaces.

Best regards,

Ladislav

0 项奖励
回复