mc9s12xep100 MSCAN

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

mc9s12xep100 MSCAN

781 次查看
chenchenchen
Contributor II

Hi,I have some problem with MSCAN. I run a program to test MSCAN,but the CAN0CTL0_SYNCH bit is always is 0, so MSCAN can not transmit anything. And I am sure that the program is right,beause run this program sucessfully in other board. So, I want to know what about reasons cause this.  Is hardware cuased this?

0 项奖励
回复
1 回复

668 次查看
lama
NXP TechSupport
NXP TechSupport

Hi,

the issue could be anywhere. Program could be OK (I are absolutely sure there a re no changes) but the system you have put your node into could be different - I do not know, you have not described.

If I were in your shoes I would:

1) check the bus clock and/or oscillator clock to be sure the CAN clock is OK. Also check all the nodes connected to the bus  use the same you are connection to

2) test the CAN in the loopback mode to be sure CAN peripheral is OK.

3) test the communication between two CAN nodes at the same MCU without transceiver to be sure the communication is OK. The circuit can be found https://www.mikrocontroller.net/attachment/28831/siemens_AP2921.pdf 

In this case I would also measure the CAN signal by the scope whether the communication speed is OK.

4) If the everything above is OK then the issue is on the transceiver side and/or BUS.

I know, it is easy to write it but difficult to test. However, it is necessary to go step by step to exclude possible sources of issues.

Best regards,

Ladislav

0 项奖励
回复