masserase memory map

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

masserase memory map

1,533件の閲覧回数
Neo_zhang
Contributor II

CW execute masserase, which part the memory has been erased?  both EEPROM and flash or just the flash ?

0 件の賞賛
返信
2 返答(返信)

1,516件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi,

Could you please specify the target MCU you are using?

In case it is S12(x) family there is an option to enable/disable erasing of EEPROM (go to File -> Configuration dialog - where you can specify which flash memory blocks should be erased:

stanish_0-1709902761322.pngstanish_0-1709902761322.png

If you use S12z the debug will erase just Program FLASH. in order to program EEPROM you should use Flash Programmer component (Target Task): 

stanish_1-1709903067485.pngstanish_1-1709903067485.png

 

Hope it helps.

Stan

 

0 件の賞賛
返信

1,513件の閲覧回数
Neo_zhang
Contributor II

My target MCU  is MC9S12DT256, can I edit 0x000 - 0x3FF registers region and 0x1000 - 0x3FFF RAM and how to do it?

0 件の賞賛
返信