looking for header files

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

looking for header files

2,213 Views
三木理人
Contributor I

 There is no following header file for the sensorless motor evaluation board (ZVM target), and an error will be generated at the time of build. Where can I get the header file below?

〇header file that i want to obtain:

         "gflib.h"  ,  "gmclib.h"  ,  "gdflib.h"

        

         

note:〇Target: S12ZVML128

〇CW ver: 10.7

〇pmp for EVA :AN5327_SW_CW10

3 Replies

1,885 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

There is the possibility that you have installed the library, so at first check C:\Freescale\AMMCLIB\...

(current version is 1.1.11) or you can download the library from the website Automotive Math and Motor Control Library Set|NXP 

Best regards,

Diana

1,885 Views
pachamatej
NXP Employee
NXP Employee

Just a comment: we have noticed a bug in the AMMCLib installer, which overwrites all the paths in installed projects to mistaken version 1.1.1. As a temporary fix, you need to go to the Project Properties -> C/C++ General -> Paths and Simbols and change all the paths linked to the AMMCLib manually. It should be fixed in this week's release.

0 Kudos
Reply

1,885 Views
pachamatej
NXP Employee
NXP Employee

Fixed :smileyhappy:

0 Kudos
Reply