Hi,
XDG is a family member of S12XD family. The attached examples are made for XDP and they are fully usable for the MCU you use. Of course it is necessary to change MCU type and include file (if necessary) to be they ported to XDG256 memory size.
I believe attached examples will lead you to correct solution.
The procedure I always suggest to be sure the can is correct is:
1) create loop-back communication at one channel
2) create communication between two channels at the same MCU without external transceiver as described in attached CAN without Transceiver-siemens_AP2921.pdf
3) use transceiver for communication between two nodes
I know the approach looks to be complicated, however in the case when you are not able to analyze communication protocol by means of scope then this approach provides you possibility to localize possible mistakes. Let's imagine you will directly start with item 3. How do you then know whether issue is in your SW or transceiver or other node.
Note> Remove extension *.ddd from the attached file and replace it by *.zip.
Best regards,
Ladislav