how to use interrupt of Freescale MC9S12G64

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to use interrupt of Freescale MC9S12G64

653 Views
user_112139582
Contributor I

Hi everyone,

      I have a trouble  when programing the timer. here is the code. I'll very gratefull.

 

 

void SetBusCLK_16M(void)

 CPMUOSC_OSCE=1;                          //enable oscillator 

CPMUCLKS_PLLSEL=0;                    //  disable   PLL

 CPMUREFDIV=0x41;    //Fref=Fosc/(1+1)=4M
 CPMUSYNR=0x03;      //  Fvco=2*Fref*(1+3)=32M 

 CPMUPOSTDIV=0x00;     //   Fpll=Fvco/0+1  =32M,Fbus=16M  

  _asm(nop);                       

  _asm(nop);
  _asm(nop);
  _asm(nop);
  while(CPMUFLG_LOCK == 0);  
  while(CPMUCLKS_PLLSEL==0);  

  CPMUPROT=0x00; 

}

 

 

void initialize_ect(void)
{
  TSCR1_TFFCA = 1;  

  TSCR1_TEN = 1;    

  TIOS  = 0xFF;    

   TCTL4 = 0x00;   
  TIE   = 0x01;     //enable channel  0 interrupt

TSCR2 = 0x87;     

  TFLG1 = 0xff;    

  TFLG2 = 0xff;    } 

  #pragma CODE_SEG __NEAR_SEG NON_BANKED  
 
void  interrupt 16_Vtimovf (void)  //   this interrupt enty is ok
{
  if(TFLG2_TOF ==1)
  {
           temp=TCNT;
    dd = ~dd;     //for LED sparking per second   
 
  }
}
#pragma CODE_SEG DEFAULT

 

 

/*************************************************************/
#pragma CODE_SEG __NEAR_SEG NON_BANKED   


void interrupt 8_Vtimch0 (void)//  This interrupt entry is wrong. WHY?
{
 
  TFLG1_C0F = 1;              

  TC0 = TCNT +125;                  
     ZZ=~ZZ;    //for out put a wave at one I/O. 

}
#pragma CODE_SEG DEFAULT

Labels (1)
0 Kudos
Reply
0 Replies