how to encrypt my source code of C language with CWS12v5.1,do CW software have this function?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to encrypt my source code of C language with CWS12v5.1,do CW software have this function?

1,982 Views
贵阳封
Contributor I

Now i have already finished my C routine with MC9S12VR series MCU ,my interface is USB mutilink ,how to encrypt my source code of C language and then download it to the MCU to prevent others illegal reading my source codes from MCU?do CW have this function?if not do other device or software own this function? who can give me some advices? thank you very  much.

Labels (1)
Tags (1)
0 Kudos
Reply
5 Replies

1,679 Views
kef2
Senior Contributor V

Source code enryption available in CW has nothing to do with MCU. Having CW PRO licence you enable encryption in project settings and compile. Instead of producing object o-files, CW compiler will produce encrypted source files which are not human readable and have file extension like *.c_e . You can give these encrypted files to your consumer and he will be able to compile them with CodeWarrior but won't be able to see C source or edit them.

MCU security is access prevention to flash and EEPROM. To enable MCU security you need to program byte at global address 3_FF0F with lowest order bits set to 00,01 or 11. See register FSEC description.

1,679 Views
贵阳封
Contributor I

Thanks for your detailed reply. But what does CW PRO licence means? it's  the Cyclone PRO device ? yes i have set the security options according to the datasheet.

0 Kudos
Reply

1,679 Views
kef2
Senior Contributor V

CW PRO license is CodeWarrior Professional Edition licence. I think source code encryption is available only with this edition.

0 Kudos
Reply

1,679 Views
贵阳封
Contributor I

Now i don't have the licence of CW Pro ,do you know other device such as Cyclone PRO have this encryption function ?

发送自魅族MX

0 Kudos
Reply

1,679 Views
kef2
Senior Contributor V

Cyclone PRO has nothing to do with source code encryption.

Regarding enabling MCU security, please check again my first reply. Yes, you can enable chip security with Cyclone PRO.

0 Kudos
Reply