getting linker error while using MC9S12XDP512 boards please help me in solving this tricky problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

getting linker error while using MC9S12XDP512 boards please help me in solving this tricky problem

2,348件の閲覧回数
saurav99
Contributor I
Hi All,
 
I am using MC9S12XDP512 boards with Code Warrior version V4.6.
I am getting linker error L1100:segments.absseg436(0X268) and .absseg651(0X268) overlap
I am getting linker error L1100:segments.absseg438(0X26A) and .absseg652(0X26A) overlap
link failed is the error.
 
why this kind of error is coming what is the cause of this error can any one help me in solving this tricky problem.It seems to be tricky every thing right and every thing got compiled no errors but this strange linker problem what might be the cause.
 
If any one helps me in getting solved this problem it would be of great help to me and great learning fom you for me.

Thanks in advance,
 
Thanks,
Saurav99
ラベル(1)
0 件の賞賛
返信
1 返信

1,258件の閲覧回数
CompilerGuru
NXP Employee
NXP Employee
As tip, search this forum for L1100.

Basically the linker tells you that there are two objects at 0X268 address. One is probably the PTJ register defined in mc9s12xdp512.c, the other one, well dont know.
Basically you apear to have in your code

unsigned char whatever@0x268;

and somewhere else

unsigned char anotherThing@0x268;

Could also be that one of the definitions is a asm ORG section.

Daniel
0 件の賞賛
返信