float calculation problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

float calculation problem

2,052件の閲覧回数
HarryHirn
Contributor I

hi guys

 

i got a problem with my hc12 and a calculation...

 

what i wanna to do: do a correlation of 2 signals

 

i found and codesnippet in an book for c# and hooked it over to my controller:

 

 

int i = 0;float sumx = 0.0;float sumy = 0.0;float sumxx = 0.0;float sumyy = 0.0;float sumxy = 0.0;float rho = 0.0;for(i = 0; i < length; i++){  sumx += x[i];  sumy += y[i];  sumxx += x[i] * x[i];  sumyy += y[i] * y[i];  sumxy += x[i] * y[i];    }rho = ((length * sumxy) - (sumx * sumy)) / (sqrtf(((length * sumxx) - (sumx * sumx)) * ((length * sumyy) - (sumy * sumy))));

 

 

the problem starts right at the beginning by calculating sumxx...

 

my x-array contains: { 1, 4, 2105,.....}

 

stepping through the function gives the sumxx values { 1, 17, -25406, ...}

 

the first two values are correct, but why does the third cracks up? should be something like 4431042... or something like 4.43102E06

 

because of the values the correlation becomes inverted, sometimes completely wrong and sometimes greater 1

 

i got another realization of a correlation implemented which calculates correctly with same values but is far more runtime unfriendly. there the values go up toe 8,xyzE07 without a problem...

 

whats the problem with summing up floats that way?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,689件の閲覧回数
kef
Specialist I

First of all, if you want to be helped next time, please provide at least all necessary declarations. Why should I guess what type is your x array? Compileable small snippet could be even better. It would dramatically ease helping you.

 

I guess x[] array is array of int's or short's. If so, then no wonder integer 2105 * integer 2105 overflows. Integer 2105 * 2105 is chopped to 0x9CB1 (-25423). Next -25423 is converted to float and added to sumxx.

To fix it change your expressions like this

 

  sumxx += (long)x[i] * x[i];

 

or this

 

  sumxx += (float)x[i] * x[i];

 

0 件の賞賛
返信

1,689件の閲覧回数
HarryHirn
Contributor I

Hi mate

 

you are right... in all you said :smileyhappy:

maybe your better in guessing than you believe :smileywink:

 

it was shortly before lunch break so i posted this in a heck hoping to be solved after lunch...

and it works...

 

changed to   sumxx += (float)x[i] * (float)x[i];

 

my array is an array of adc values in int, so there the overflow happened. with the cast it works.

 

next time i will provide more informations :smileyhappy:

 

0 件の賞賛
返信