first code = problem (9s12c32)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

first code = problem (9s12c32)

4,151 Views
bluemind
Contributor I

im a newbiem and this is my first code, so bear with me, the only thing it shal is to make a led blink. (running one a DF12-DIP40-R, on a DF12-DOCK40(www.evbplus.com))

 

im using CW! do it loock totally off....

 

do i need to set the pll to run prorgams on the chip. and if so, where can i find code there will work.

 

my problem is that i am missing examples/information in how to program in c. almost all i can find is in assamble, and i¨m not good at that. posserbil a good book to read on the subjekt woud be great..

Labels (1)
0 Kudos
Reply
2 Replies

1,861 Views
kwik
Contributor I

Did you download Englers or Franks IDE's ? You find links at www.evbplus.com

When you do that you will find example projects in C .

An example project is even better than books.....

0 Kudos
Reply

1,861 Views
bluemind
Contributor I
found the problem...

but are there any book you woud recomand for a newbie.
0 Kudos
Reply