external EEPROM with a MC9S12P64VLH?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

external EEPROM with a MC9S12P64VLH?

804 次查看
marchandthomas
Contributor I

Hello ,

 

do you know if there is an existing schematic for connect an external EEPROM with a MC9S12P64VLH?

I think we can use a ATMEL25640 on the Pin 58 ,57,56,55 (MISO0,/SSO,MOSI0,/SCK0). Do you know the best circuit?

Thanks you.

标签 (1)
标记 (2)
0 项奖励
回复
1 回复

737 次查看
iggi
NXP Employee
NXP Employee

Hi,

The S12P features SPI module (MISO0,/SSO,MOSI0,/SCK0) as well, so you can use this serial interface for external EEPROM.

Below post can be of help as an alternative:

External Serial EEPROM | Freescale Community

Moreover, there is an appnote for S12P devices about EEPROM emulation (it comes with the SW driver), so you might not need to use external EEPROM:

AN4483, Emulated EEPROM Routines for the S12P Family - Application Notes

AN4483SW

Regards,

iggi

0 项奖励
回复