#define MODRR0_S0L0RR_MASK   7U

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

#define MODRR0_S0L0RR_MASK   7U

1,274 次查看
sufree
Contributor II

Hi,

    The following code are in "mc9s12zvmc128.h" file .I can't find the define of 7U,0U,8U and so on .I don't know the meaning of it.   Who can give me a little hint ?

 

#define MODRR0_S0L0RR_MASK   7U
#define MODRR0_S0L0RR_BITNUM   0U
#define MODRR0_SCI1RR_MASK   8U

标签 (1)
0 项奖励
回复
1 回复

1,150 次查看
RadekS
NXP Employee
NXP Employee

Hi 歌 苏,

Please see MODRR0 Routing Register description in chapter 2.3.2 PIM Registers 0x0200-0x020F in RM.

The MODRR0_S0L0RR_MASK and MODRR0_SCI1RR_MASK are just masks.

So, if you calculate MODRR0 & MODRR0_SCI1RR_MASK it will return SCI1 routing setting to you, despite on other bits in MODRR0 register.

The SCI1 routing options are presented by just one bit - SCI1RR

The SCI0 routing options are presented by three bits - S0L0RR[2..0]

 

The default SCI0 routing option is 0b000 = 0x00 = 0 (MODRR0_S0L0RR_BITNUM). In that case the SCI0 is internally connected to LINPHY0/HVPHY0.

See Table 2-10. Preferred Interface Configurations for more details.

 

Note: The MODRR0 register might be written just once in normal mode. So, all settings have to be managed by singe write into this register. For example:

Correct:

MODRR0=0x80; //SCI0 internal, SCI1 to PS2,3, SPI0 to PS2..4, SPI0 SS0 at SP5

Wrong:

MODRR0_S0L0RR = 0x00; //SCI0 internal

MODRR0_ SCI1RR = 1; //SCI1 to PS2,3

MODRR0_SPI0RR = 0; //SPI0 to PS2..4

MODRR0_SPI0SSRR = 0; //SPI0 SS0 at SP5

I hope it helps you.

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复