current Consumption S12ZVH

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

current Consumption S12ZVH

1,119件の閲覧回数
rajnirajpoot
Contributor II

Hi i am using s12zvh128 in one of our project.

Following are the peripherals used :-

LCD Module

ADC

Motor Control

Pwm

Timer

Capture

For Lcd clock i am using rtc clock as internal clock source.

On ignition off i have to reduce the current so for that i disable all the peripherals just enable one timer of 100ms for digital clock display on lcd . I can't put MCU in stop mode as accuracy of clock is disturbed . what can i do for further reduction in current?

How to off internal reference clock?

0 件の賞賛
返信
1 返信

1,044件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi

I think you can use Wait Mode instead of Stop Mode.

I this mode, RTC, Timer and LCD can continue to operate while the CPU in a standby state.

Regards,

Daniel

0 件の賞賛
返信