communication with the target failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

communication with the target failed

4,370件の閲覧回数
nathan_
Contributor IV

I use MC9S12XS128.I have a P&E Multilink. The program can be downloaded only a few times, then the communication with the target failed. The P&E Multilink and the chip has no problem. what's the problem? is there problems with the circuit?

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

4,166件の閲覧回数
iggi
NXP Employee
NXP Employee

Hi,

what board do you use? is it Freescale or you custom made?

Can you share the schematic for review?

Regards,

iggi

0 件の賞賛
返信

4,166件の閲覧回数
takaoyamada
Contributor IV

Greetings,

1) What software are you using?

2) Do you secure the chip? It is possible the chip is secured and you can unsecure it using P&E's unsecure_12 utility:
http://www.pemicro.com/downloads/download_file.cfm?download_id=16

3) Are both blue and yellow LED on the multilink lit? If the blue is not lit, then the computer recognizes the multilink. The yellow indicates it detects power on your target board.

Takao Yamada

P&E Microcomputer Systems

0 件の賞賛
返信

4,164件の閲覧回数
nathan_
Contributor IV

I am using code warrior v5.1.

I did not secure the chip, but sometimes the program just can not be downloaded to the chip.

The two LED are both lit.

I wonder if the circuit around the chip has some problems. It’s bothering me.

发件人: [email protected] 代表 takaoyamada

发送时间: 2015年5月11日 21:50

收件人: nathan ?

主题: Re: - communication with the target failed

<http://jiveon.jivesoftware.com/mpss/c/hQA/PDcDAA/t.1mx/h9IU3Fj5QQG32O4nPvzA0Q/h0/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bQ-3D>

communication with the target failed

reply from Takao Yamada <http://jiveon.jivesoftware.com/mpss/c/hQA/PDcDAA/t.1mx/h9IU3Fj5QQG32O4nPvzA0Q/h1/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bSuCNbcudobw38Sw1SacfMl6IgOJVhGnluq4sFznI9DFQFuR1n8F5xufT7dZQ9Eju0-3D> in 16-bit Microcontrollers - View the full discussion <http://jiveon.jivesoftware.com/mpss/c/hQA/PDcDAA/t.1mx/h9IU3Fj5QQG32O4nPvzA0Q/h2/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bSN285yELqScS0EM1C5-2F91iU8KbAfpL3EFr4Px-2FngBZJiCAIFstntKpXUxYDLenNmM-3D>

0 件の賞賛
返信