communication between MC9S08LG32 and HCS12

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

communication between MC9S08LG32 and HCS12

1,737件の閲覧回数
Yuping
Contributor I

Hi All,

 

Has anyone tried communicating between the 8-bit processor and the 16-bit processor? I am trying to connect these two processors for a project, but couldn't figure out how to do that. Could anyone help?

 

Thanks!

 

Btw, I am posting this message on both forums, 8-bit MCU and 16-bit MCU. If this is not allowed, I apologize for doing this, and please feel free to delete one of them...

 

Yuping

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,415件の閲覧回数
bigmac
Specialist III

Hello Yuping,

 

The following thread discusses a method of communicating between two MCU, in this case two HCS12 types.  The method would also be applicable where one device is an 8-bit MCU.

https://community.freescale.com/thread/66448

 

Regards,

Mac

 

0 件の賞賛
返信

1,415件の閲覧回数
Yuping
Contributor I

Hi Mac,

 

Thanks for your help! I'll give it a try. I'll ask more questions if I encounter any problem.

 

Thanks,

Yuping

0 件の賞賛
返信