capture counter for HCS12X

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

capture counter for HCS12X

908 次查看
lin_karl
Contributor I

currently I am using CodeWarrior to develop HCS12X MCU and I need it to capture a time between two edges. so I am using capture function to accomplish this task.

 

        right now  I have two timers, 1 ms and 1 us and the max counter(max time of event)  for capture is 32768 us.  so when I receive a value from capture, on which does the capture counter base?

 

for exampl, if I receive 100 from capture counter, does it mean 100 ms or 100 us? 

 

thanks, 

 

carl 

标签 (1)
0 项奖励
回复
0 回复数