bootloader tutorial

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

bootloader tutorial

2,446 Views
mojtaba_al22
Contributor II

Hello to all;

i have a project with s912g128mll and i want to add bootloader codes to update my firmware By the customer.

Please tell me where to start.

Labels (1)
0 Kudos
Reply
3 Replies

2,239 Views
mojtaba_al22
Contributor II

But let's also say that I need to use the CAN protocol to update.

0 Kudos
Reply

2,239 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

Unfortunately, there is no CAN bootloader for the S12G device. However, the links below can be helpful.

Useful documents for building own CAN bootloader 

Also, this question has already been discussed, please, refer to additional notes in this community thread:

S12 can bootloader ask for help! 

The MSCAN driver can be downloaded here: https://www.nxp.com/webapp/Download?colCode=MSCAN_S12_DEVD 

I hope it helps.

Best Regards,

Diana

0 Kudos
Reply

2,239 Views
mojtaba_al22
Contributor II

hello Diana 

Thank you for your post. I will definitely check 

Best Regards,

Mojtaba

0 Kudos
Reply