adc conversion time setting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

adc conversion time setting

2,569件の閲覧回数
jyothipusuluri
Contributor I

Hi all, for xep100 micom, how to achieve adc conversion time of 3.2us?(please suggest me how to calculate conversion time from ATD clock cycles,if my prescale value is 3,sample time scale 000,ADC resolution is 12bit) jyothi Pusuluri

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,092件の閲覧回数
kef2
Senior Contributor V

You didn't specify ATD clock source frequency, so I can't suggest specific figures. Check table A-15  ATD Operating characteristics and note 2 under that table. For 12bits resolution, conversion time (including sample time) is from 20 to 42 ATD clock cycles. That's num of sample time clocks + 16. When discharge (SMP_DIS) is enabled, conversion time takes longer, plus additional 2 ATD clock cycles.

12bits: sample clocks + 16 + SMP_DIS*2

10bits: sample clocks + 15 + SMP_DIS*2

8bits: sample clocks + 13 + SMP_DIS*2

Hope this helps.

2,092件の閲覧回数
iggi
NXP Employee
NXP Employee

Hi,

The total conversion time can be calculated as follows:

Total Time = conversion time + sample time + discharging time


Conversion time:

12bit resolution: 16 ATDCLK cycles

10bit resolution: 15 ATDCLK cycles

8bit resolution: 13 ATDCLK cycles

Sample time: can be set in range 4 – 24 ATDCLK cycles

Discharging time:

If bit SMP_DIS in ATDCLT1 register is set then it takes 2 ATDCLK cycles.

If SMP_DIS is 0 then it takes 0 ATDCLK cycles.

So, min/max times in case of 12bit resolution is:

Minimum time = 16 + 4 + 0 = 20 ATDCLK cycles

Maximum time is: Time = 16 + 24 + 2 = 42 ATDCLK cycles

ATDCLK can be set in range 0.25 – 8.3MHz.

Depending on the MCU bus clock and equation to calculate the ATD clock which is:

fATDCLK = fBUS / 2×(PRS + 1)

you can easily calculate ATDCLK cycles in microseconds.

Regards,

iggi

0 件の賞賛
返信