access problems to target with USB P&E and MC9S12XDP512

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

access problems to target with USB P&E and MC9S12XDP512

Jump to solution
2,136 Views
chris69
Contributor I

Hi,

 


I was programming my MC9S12XDP512  with the P&E USB multilink and PROG12Z, it worked fine.

 

But this mornig, i did a mistake, i launched PROG12Z, i choose my alogrithm, and instead of click on "erase module", i clicked on "blank check module".

 

 

So i stoped the process in the middle of the operation, and i cliked on "erase module", but the operation began et never stoped. So i closed the soft, and now i can't connect my proceesor; each time i launch PROG12Z,  i have the message "Can't communicate with the target processor.Target processor may be  secure, unpowered or not properly connected".

 

 

Can anybody give me a hint how I can gain access to the target again?

Labels (1)
0 Kudos
Reply
1 Solution
1,471 Views
kef
Specialist I

Did you try to unsecure with P&E unsecure12 utility? You can download it from www.pemicro.com .

IO_DELAY_CNT setting is quite weird. Shouldn't it be 240/ oscilator frequency?

View solution in original post

0 Kudos
Reply
2 Replies
1,472 Views
kef
Specialist I

Did you try to unsecure with P&E unsecure12 utility? You can download it from www.pemicro.com .

IO_DELAY_CNT setting is quite weird. Shouldn't it be 240/ oscilator frequency?

0 Kudos
Reply
1,471 Views
chris69
Contributor I

Thank you kef,

 

My problem was my processor was secure, I unsecure it with Codewarrior.

 

thak you again.

0 Kudos
Reply