a bootloader question  for freescale 12xet256 microcontroller

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

a bootloader question  for freescale 12xet256 microcontroller

2,180件の閲覧回数
blin
Contributor I

I 'm new in writing a bootloader for freescale 12xet256 microcontroller,I  get from the newer application note AN4258 Serial Bootloader for S12(X) Microcontrollers Based on 180 nm Technology

 

 

I meet two questions:

 

first:i use demo AN4258 ,but dont dowmload program via TBDML,the computer show "Error while writing to FD00..FF00" 

second  : i replace TBDML, use USB Multilink Universal FX ,unfortunately   codeworrior5.1 can't recognise the tool,

            show "undected Disconnect/connect USB cable. click Refresh list"

 

 

please help me,thank you!

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,015件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Hi,

What do you really want to download? Is it Bootloader or Bootloader merged with an application?

What procedure have you used? (Please refer to an AN4258 pages)

Mutilink Universial FX doesn't support classic Codewarrior for HCS12. It only supports CW10.2 and higher. See this url:

http://www.pemicro.com/products/fx_software.cfm

to work with CW5.1, please use

USB BDM Multilink Cable:

http://www.pemicro.com/products/product_viewDetails.cfm?product_id=33

Or

USB Multilink Universal:

http://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320137

Best regards,

Ladislav

0 件の賞賛
返信

2,015件の閲覧回数
kef2
Senior Contributor V
0 件の賞賛
返信