ZVC bootloader

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ZVC bootloader

1,786 次查看
xiaohui200808
Contributor III

Hello

     I make a bootloader on one project.In app I donot use the interrupt .It could work normal (include update app).But when my app use the interrupt .I relocated the interrupt table.when I download it By Multilink .app(boot and app are in one project ) could work normally. But when I update the app ,it can not work normally .I read the Flash ,the S19 which I download ,are right .when  reloacated the interrupt table ,need there something to prepare. Attenchment is my code .Please help me check it . 

Original Attachment has been moved to: New_S12ZVC_Boot123.zip

标签 (1)
0 项奖励
回复
1 回复

1,474 次查看
RadekS
NXP Employee
NXP Employee

Hi Xiaohui,

Please look at our conversation in your previous thread:

https://community.nxp.com/message/870851

I hope it helps you.

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复