XGATE with 29-bit identifier CAN.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

XGATE with 29-bit identifier CAN.

1,914件の閲覧回数
memismo
Contributor I
Hi everyone,
 
I have read several XGATE documentation (Fact Sheet, Introducing, CAN driver, ...) and I'm not sure that i can use XGATE with 29- bit identifier CAN, i believe the documentation it´s too embarrassed.
 
Can anyone help me????
ラベル(1)
0 件の賞賛
返信
1 返信

1,066件の閲覧回数
Lundin
Senior Contributor IV
Yes you can the XGATE with 29-bit CAN identifier, otherwise it wouldn't be CAN.

The only difference the mcu makes between 11 and 29 bit is that if you are using the message masks and filters, you need to set them for either 11 or 29 bit. If you don't use either, you don't need to worry about it at all.

What do you mean with "embarrassed documentation"? It is written by engineers for engineers, so it won't exactly be masterpiece fiction. It contains all you need to know though: if you are an engineer who knows CAN, you shouldn't have any trouble understanding it.
0 件の賞賛
返信