XGATE semaphore question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

XGATE semaphore question

Jump to solution
3,218 Views
roberthiebert
Senior Contributor I

MC9S12XEP100, CW Special Edition, USBDM, XGATE in RAM, coding in relocatable assembler.

I have a project that was written in absolute assembler which uses a lot of interrupts. It runs just fine now, but I want to incorporate XGATE to handle most, if not all of the interrupts. Why? Probably just to see if I can. To that end, I have been able to convert the project to relocatable assembler, (which wasn't easy for me) but it seems to work.

Anyway, I spend a lot of time studying the reference manuals and AN2685, but I 'm still not quite clear on the basics of XGATE semaphores. 

When I change an interrupt service routine to be serviced by XGATE instead of the CPU, I have read that semaphores need to be involved, but I m not clear under just what circumstances.

Do they need to be used just when a variable is modified within an ISR serviced by XGATE, and, modified by an ISR service by the CPU?

Or.

Also, when a variable is modified within an ISR serviced by XGATE, but it is only used by the CPU, but not modified?

Regards,

Robert 

0 Kudos
Reply
1 Solution
3,189 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

Semaphores are needed only when both cores (S12X and XGATE) access the same shared resource, typically a variable in RAM. The are needed to avoid simultaneous R/W from both cores. For example, CPU writes some data in one or two steps and XGATE reads them at the same moment. Data consistency is not guaranteed.

 

Use semaphores when:

  1. A variable is modified by both XGATE and S12X ISRs.

Example: A status flag or counter updated by both cores. Or writing to a port.

  1. A variable is modified by one core and read by the other, and the read must be consistent.

Example: A buffer index updated by XGATE and read by S12X in a loop.

You do not need semaphores when:

  • A variable is only modified by XGATE, and only read by S12X, and consistency is not critical (e.g., occasional stale reads are acceptable).
  • A variable is only accessed by one core (either read or write).

 

Note, I found in my old code following. It is probably not important for some mask sets but better to implement to be sure it works everywhere.

....  *.cxgate module

interrupt void PIT0isr(void)

{

      //--- Protected software region starts     // AN2685.pdf

     //-----------------------------------------

      // use this

      asm LOOP1:

      asm SSEM #0 // try to lock semaphore 0

      asm SSEM #0 // try to lock semaphore 0     // once more due to internal silicon bug

      asm BCC LOOP1 // retry if locked

      //-----------------------------------------

      //or this

      //asm SSEM #0 // try to lock semaphore 0

      //asm SSEM #0 // try to lock semaphore 0     // once more due to internal silicon bug

      //asm BCC PIT0isr_RTI // return without flag clearing to enable service of an interrupt with higher priority

      //-----------------------------------------

 

    ....

    .....

    ....

      //-----------------------------------------
      asm CSEM #0 // release semaphore
      //-----------------------------------------

asm PIT0isr_RTI:

      //-----------------------------------------
      PITTF = 0x01; // clear interrupt flag of PIT0isr

}

Best regards,

Ladislav

View solution in original post

0 Kudos
Reply
2 Replies
3,190 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

Semaphores are needed only when both cores (S12X and XGATE) access the same shared resource, typically a variable in RAM. The are needed to avoid simultaneous R/W from both cores. For example, CPU writes some data in one or two steps and XGATE reads them at the same moment. Data consistency is not guaranteed.

 

Use semaphores when:

  1. A variable is modified by both XGATE and S12X ISRs.

Example: A status flag or counter updated by both cores. Or writing to a port.

  1. A variable is modified by one core and read by the other, and the read must be consistent.

Example: A buffer index updated by XGATE and read by S12X in a loop.

You do not need semaphores when:

  • A variable is only modified by XGATE, and only read by S12X, and consistency is not critical (e.g., occasional stale reads are acceptable).
  • A variable is only accessed by one core (either read or write).

 

Note, I found in my old code following. It is probably not important for some mask sets but better to implement to be sure it works everywhere.

....  *.cxgate module

interrupt void PIT0isr(void)

{

      //--- Protected software region starts     // AN2685.pdf

     //-----------------------------------------

      // use this

      asm LOOP1:

      asm SSEM #0 // try to lock semaphore 0

      asm SSEM #0 // try to lock semaphore 0     // once more due to internal silicon bug

      asm BCC LOOP1 // retry if locked

      //-----------------------------------------

      //or this

      //asm SSEM #0 // try to lock semaphore 0

      //asm SSEM #0 // try to lock semaphore 0     // once more due to internal silicon bug

      //asm BCC PIT0isr_RTI // return without flag clearing to enable service of an interrupt with higher priority

      //-----------------------------------------

 

    ....

    .....

    ....

      //-----------------------------------------
      asm CSEM #0 // release semaphore
      //-----------------------------------------

asm PIT0isr_RTI:

      //-----------------------------------------
      PITTF = 0x01; // clear interrupt flag of PIT0isr

}

Best regards,

Ladislav

0 Kudos
Reply
3,172 Views
roberthiebert
Senior Contributor I

Hi Ladislav,

Thanks for the clarification. That's how I thought it should work, but I wasn't sure.

Regards,

Robert

0 Kudos
Reply