Would you please provide to me PI control algorithm with source code?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Would you please provide to me PI control algorithm with source code?

ソリューションへジャンプ
1,609件の閲覧回数
jtpark
Contributor IV

Hello,

 

I tested s/w for DC motor control with S12ZVC.

I have to use PI control algorithm.

Would you please provide to me it for source code?

 

Thank you.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,431件の閲覧回数
RadekS
NXP Employee
NXP Employee

Hi J.T.

The PI control algorithm is part of our AMMCLib - Automotive Math and Motor Control Library Set

http://www.nxp.com/products/software-and-tools/run-time-software/automotive-software-and-tools/motor...

The source code as C/ASM code is not included in evaluation version, but you will get it when you buy a license.

I hope it helps you.

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,432件の閲覧回数
RadekS
NXP Employee
NXP Employee

Hi J.T.

The PI control algorithm is part of our AMMCLib - Automotive Math and Motor Control Library Set

http://www.nxp.com/products/software-and-tools/run-time-software/automotive-software-and-tools/motor...

The source code as C/ASM code is not included in evaluation version, but you will get it when you buy a license.

I hope it helps you.

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------