Why  the  mc9s12zvm128  microcontroller  is  easy  to  damage

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why  the  mc9s12zvm128  microcontroller  is  easy  to  damage

858 Views
pengweiyes
Contributor I

I am use the MC9S12ZVM128  microcontroller .

In the process of application I find the Mc9s12zvm128’s VBS0~VBS3 are  easy to damage, Circuit diagram is as follows:

148276_148276.pngpastedImage_0.png

Labels (1)
0 Kudos
Reply
1 Reply

738 Views
RadekS
NXP Employee
NXP Employee

Hi 伟 彭,

I would like to recommend an optional RC filter to VBS pin (for all three phases) that it be used to avoid overshoot above the maximum voltage on VBS pin. The RC filter needs to be carefully designed in order not to influence the charging time of the bootstrap capacitor CBS.

Optional RC filter to VBS pin.png


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply