Why I must set the Port P to output mode when I want use the SPI module?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why I must set the Port P to output mode when I want use the SPI module?

1,621件の閲覧回数
xiangtailiang
Contributor I
I got a very magical problem that I can slove by myself.
I need your help...Thank you!
Device: 9S12XS128 80pin
IDE:   Codewarrior 5.0 
Problem:
When I use SPI Master mode,my initial code as below doesn't work:
  MODRR = 0x10; //spi use m4 m5 port
  (void)SPI0SR; /* Read the status register */
  (void)SPI0DRL;  /* Read the device register */ 
  SPI0CR1 = 0x50;
  SPI0CR2 = 0x08;
  SPI0BR = 0x01;
But when I set the Port P to output mode,just like this:
  DDRP=0XFF; //Set Port P to output mode               
  MODRR = 0x10; //spi use m4 m5 port
  (void)SPI0SR; /* Read the status register */
  (void)SPI0DRL;  /* Read the device register */ 
  SPI0CR1 = 0x50;
  SPI0CR2 = 0x08;
  SPI0BR = 0x01;
It can work very perfectly now.
What happen?Why I must set the Port P to output mode when I want use the SPI module?
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

976件の閲覧回数
Lundin
Senior Contributor IV
Since you aren't setting SSOE in SPICR1, the MCU expects you to handle SS manually. If SS is an input, nothing will work as the slave will never get a chip select. Instead of setting DDRP, try setting SSOE.
0 件の賞賛
返信

976件の閲覧回数
xiangtailiang
Contributor I

Thanks for your help, I have try to set the SSOE in SPI0CR1. But it dosen't work.

 

0 件の賞賛
返信

976件の閲覧回数
Lundin
Senior Contributor IV
I just realized that you might have to set the MODFEN bit too to get it to work. But instead of relying on some stranger on a message board, I'd strongly recommend to read the register descriptions in the manual. :smileyhappy: Whether you can use SSOE or not depends on the device you are speaking with. You will have to check timing diagrams etc in the data sheet. I know there are many devices that are too slow to function with the SSOE feature.
0 件の賞賛
返信