Which headerfile for mc9s12c32?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Which headerfile for mc9s12c32?

2,340件の閲覧回数
Dietrich
Contributor II

This message contains an entire topic ported from a separate forum. The original message and all replies are in this single message. We have seeded this new forum with selected information that we expect will be of value to you as you search for answers to your questions.

 

Posted: Wed Jan 26, 2005 5:31am

 

Subject: Which headerfile for mc9s12c32? 

 

    Hello!

Which headerfile must be include for an mc9s12c32?
I will use PORTT and this one is't defined in mc9s12c32.h?

Exist there an other headerfile i can use?

Thanks for help!
---------------------------------------------------------------------

Posted: Wed Jan 26, 2005 5:50am


I don't know what compiler you are using. If you are using
Codewarrior, it is defined in that h-file, as the correct name PTT.

Note that Motorola has messed up the register names a bit:

Ports A,B and E are called PORTA, PORTB, PORTE, PORTK.
They are external bus ports, check manual "MEBI".

Ports T,S,M,J,P,H are called PTT, PTS, PTM, PTJ, PTP, PTH.
They belong to port integration module, check manual "PIM".
 
---------------------------------------------------------------------

Posted: Wed Jan 26, 2005 6:24am

 
    That was it!

ラベル(1)
0 件の賞賛
返信
0 返答(返信)