Which EVMs I need to purchase to setup LIN bootloader in MM9Z1J638.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Which EVMs I need to purchase to setup LIN bootloader in MM9Z1J638.

跳至解决方案
1,619 次查看
churyjeong
Contributor II

Question) How to setup a test system for MM9Z1J638 LIN Bootloader

LIN_Bootloader.JPG

Dear who may concern about this issue, 

I'd like to setup a test environment for LIN bootloader on MM9Z1J638. 

Currently, I have a KIT9Z1J638EVM Board. 

My target is to download IBS application code(Motorolar S-rec image) into the KIT9Z1J638EVM via LIN. 

I'm not familiar with S12Z MCU and LIN protocol yet, so I'd like to setup a bootloader system like the picture above with the exist EVB board.

 

Could you please recommend which EVM boards I need to purchase to learn and practice myself the LIN bootloader, (Master-node and Slave-node both at the same time) ? 

I'd like to purchase Demo programs with the EVMs too. 

First of all, I'd like to learn "LIN bootloader" by following the quick-start guide with the demo program, without any change by myself. 

Many thanks in advance. 

 

2018-01-18

Additional question: 

#1)  If I purchase two sets of "S12ZVL" EVM from the link below, 

 DEVKIT-ZVL128: Development Board for ZVL128|NXP https://www.nxp.com/products/processors-and-microcontrollers/additional-processors-and-mcus/8-16-bit...

Is it possible to configure the first one as a Master-node and  the second one as a Slave-node with the different SW ? 

And where can I get the bootloader SW for Master-node, and bootloader SW for Slave-node ? 

标记 (1)
0 项奖励
回复
1 解答
1,349 次查看
churyjeong
Contributor II

Thanks for the confirmation. 

BRs

Chury 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,350 次查看
churyjeong
Contributor II

Thanks for the confirmation. 

BRs

Chury 

0 项奖励
回复
1,349 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,

Since the Figure 2 is taken from AN5389 S12Z MagniV LIN Bootloader, I assume you have already come across this application note.

The software can be found at this address: https://www.nxp.com/docs/en/application-note-software/AN5389SW.zip

It includes software for both the master and the slave ported on S12ZVL128.

So, you can use DEVKIT-ZVL128.

 

I’m not aware of any LIN bootloader ported directly on MM9Z1J638.

 

Regards,

Daniel