Which Codewarrior is needed for HCS12X in 32 and 64 bit Windows 10?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which Codewarrior is needed for HCS12X in 32 and 64 bit Windows 10?

1,799 Views
AndersJ
Contributor IV

I use CW 4.7 for HCS12X, running on Windows XP.

V4.7 has problems installing in W10.

Which CW do I need for HCS12X in 32 and 64 bit Windows 10?

Tags (2)
0 Kudos
Reply
3 Replies

1,611 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello Anders,

You should use CodeWarrior v5.2 which is working in the Windows 10:

CodeWarrior® Dev Tools for HCS12(X) MCUs | NXP 

Version 5.2 does not support some devices from older versions. However, there is a possibility to add missing derivatives.

Which MCU do you have? 

I hope it helps.

Best Regards,

Diana

0 Kudos
Reply

1,611 Views
AndersJ
Contributor IV

I use HCS12XEP100.

Where can I download V5.2?

Will my current license file work with V5.2?

0 Kudos
Reply

1,611 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello Anders,

The CW version 5.2 supports S12XEP100 MCU. You can download it on this link:

CodeWarrior® Dev Tools for HCS12(X) MCUs | NXP

Unfortunately, licensing questions are out of my supported area.
I recommend you to ask on the software licensing community:

Software Licensing 

I hope it helps.

Best Regards,

Diana

0 Kudos
Reply