Where could find demo code based on single-shunt for S12ZVM-EFP?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where could find demo code based on single-shunt for S12ZVM-EFP?

2,288件の閲覧回数
peter_shi
Contributor II

There are three current sampling methods whichusesshunts in inverter legs as current sensors,tri-shunt,dual-shuntandsingle-shunt. S12ZVM-EFP supportsdual-shunt and single-shunt.
There are two demo projects, one is for dual-shunt and another one is for single-shunt.

0 件の賞賛
返信
4 返答(返信)

1,978件の閲覧回数
sunkemiao2021
Contributor I

above address which aboat  download the code AN5327SW is error.I can not open it.Who can tell me the right address. thanks

0 件の賞賛
返信

2,182件の閲覧回数
peter_shi
Contributor II

EFP demo code has improved the startup performance as below based on dual shut sampling. AN5327 is an old software. Did you have single shut sampling for good startup performance?

Dedicated optimized for fuel pump application to achieve robust and fast start up. It meets the
strict start up condition < 150 ms from standstill to the rated speed

0 件の賞賛
返信

2,182件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

The SW for the AN5327 which is mentioned on the S12ZVM-EFP site https://www.nxp.com/design/development-boards/automotive-motor-control-development-solutions/magniv-...  

can be downloaded from this link:

http://www.nxp.com/files/microcontrollers/doc/app_note/AN5327SW.zip 

However, I would like to mention that this SW is for the MTRCKTSPNZVM128|Development Kit S12 MagniV | NXP 

 I hope it helps.

Best regards,

Diana

0 件の賞賛
返信