What is startup data structure for S12ZVM and How it gets intialised ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What is startup data structure for S12ZVM and How it gets intialised ?

913 次查看
ameykhatavkar
Contributor III

Hi,

 

While going to the start up code I come across the startupData structure.

 

*********************************************************************************************

STARTUP SECTION

---------------------------------------------------------------------------------------------

Entry point: 0xFE004F (_EntryPoint)

_startupData is allocated at 0xFE00A2 and uses 20 Bytes

extern struct _tagStartup {

  unsigned nofZeroOut     1

  _Range   pZeroOut       0x1200     62

  _Copy    *toCopyDownBeg 0xFE052A

  int      nofInitBodies  0

  _Cpp     *initBodies    0xFE00BD

  int      nofFiniBodies  0

  _Cpp     *finiBodies    0xFE00BD

} _startupData;

 

I understood the code, but I would like to know that, how it gets initialized?

Who is responsible for the same?

And is it always located at address 0xFE00A2 ?

Also Is EntryPoint address (0xFE004F is always same?

 

Regards,

Amey

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

752 次查看
RadekS
NXP Employee
NXP Employee

Hi Amey,

Please check start12z.c and start12z.h file in your project/Project Settings/Startup_Code.

This structure is used for initialize RAM prior start main() routine. The default bare metal project execute _Startup() function after reset. This _Startup() function will erase and initialize RAM.

Note: If you use ProcessorExpert, the reset vector points to _EntryPoint() instead of _Startup() .

Startup code is placed by linker, therefore location of this code could vary according linker settings and your project size.  

Note: prm linker file is in your project/Project Settings/Linker_Files.

You could try for example specifying some part of RAM and filling them by some pattern. For example:

RAM3          = READ_WRITE  0x003000 TO 0x003FFF FILL 0x33;

In that case startup code will initialize this part of RAM prior enter into main() function.

The similar way you could also copy some code from flash into RAM (RELOCATE_TO).

See "c:\Freescale\CW MCU v10.6\MCU\Help\PDF\MCU_Build_Tools_Utilities.pdf" document for more details.


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复