What is Flash page size in controller MC9S12XDP512?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is Flash page size in controller MC9S12XDP512?

1,785 Views
sanjivani
Contributor I

I am writing  Flash Driver for MC9S12XDP512.

I have query regarding Flash page size for MC9S12XDP512.

 

Query: What is Flash page size in controller MC9S12XDP512?

My Flash driver only provides page/pages write operation.

 

 

In MC9S12XDP512 controller datasheet only sectors are defined for 512K flash module.

No page is defined. Sector size is 1KBytes.

Sector size has to be an integer multiple of the page size.

 In Burst programming 64 words in a row can be programmed consecutively using command pipeline operation.

So is this Burst programming mode related to Flash Page size?

 Thanks  In Advance!!!

Labels (1)
0 Kudos
Reply
1 Reply

919 Views
chary
Contributor I

Dear Sanjivani,

I think ur having the answer with you , since flash size is 512K and you know that sector size is 1k.

now find how many pages are there in flash?

it has 32 pages (0xE0---0xFF) so u wil get size of flash page which is 16K.

al d best

0 Kudos
Reply