WATCHDOG problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

WATCHDOG problem

1,622 Views
StopMode
Contributor I

Dear All, I have a problem. I'm using the watch dog during my application works. When I want to stop the urocontroller I should be stop the watchdog but I can't do it. How Can I stop the watchdog while the uc is stop?

Kind regards

Labels (1)
0 Kudos
Reply
1 Reply

1,124 Views
kef
Specialist I

What MCU? Pseudostop or full stop mode? You can't turn COP when you want since COP divider is write once in normal operating modes. In full stop COP should be always stopped. In pseudostop COP can be enabled setting PLLCTL PCE bit. But PCE should be 0 by default and COP should be disabled also in pseudostop mode.

0 Kudos
Reply