Using SRecCvt-GUI,No output??

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using SRecCvt-GUI,No output??

1,647 Views
moking
Contributor I

I just want to use the SRecCvt-GUI to convert the Project.abs.s19 file for CAN-BootLoader(xep100) using.But when I do like the follow :

173258_173258.pngQQ截图20161221131950.png

then click convert,but no output file. I just donot why.Hope your answer.

Labels (1)
1 Reply

1,438 Views
RadekS
NXP Employee
NXP Employee

Hi Chuan,

Appears there any error/ok message when you click on Convert button?

Please check whether you have write access to this directory.

 

Are you sure that your Project.abs.s19 contains S-record data with addresses in Linear format?

By default, the CW generate an S19 file with addresses in Banked format. The Linear address format is typically used for generating *.glo files.

 

 

You may press Ctrl button and start SRecCvt-GUI.exe file. This will start SRecCvt in Debug mode (You will see Debug Command window). This may help you tracking down a source of the issue (error code, when you click on Convert button).

I hope it helps you.

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------