Unsecuring MC9S12XEP100MAG

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unsecuring MC9S12XEP100MAG

ソリューションへジャンプ
3,509件の閲覧回数
zegeyealemu
Contributor III

Good Afternoon All,

 

I tried to program the MC9S12XEP100 device with a wrong S19 file and ended up securing it.

In order to unsecure the device I used the following utility, P&E_Multilink_USB_Erase_unsecure_hcs12xe.cmd, but this seems not to work. I have used this utility for the 80 pin (MC9S12XEQ512) device previously and has worked well. I assume that there is probably another similar executable that I can use. Would you please let me know if a similar type of utility exist or any other solution.

 

Thank you in advance for your continuous help and support.

 

Best regards,

Ziggy

ラベル(1)
タグ(1)
1 解決策
3,112件の閲覧回数
zegeyealemu
Contributor III

Good Morning,

I was able to unsecure the device from the debugger (menu HC12MultilinkCyclonePro -> Unsecure...).

Thanks,

Ziggy

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,113件の閲覧回数
zegeyealemu
Contributor III

Good Morning,

I was able to unsecure the device from the debugger (menu HC12MultilinkCyclonePro -> Unsecure...).

Thanks,

Ziggy

0 件の賞賛
返信
3,112件の閲覧回数
RadekS
NXP Employee
NXP Employee

Hi Ziggy,

The menu HC12MultilinkCyclonePro -> Unsecure... just run the P&E_Multilink_USB_Erase_unsecure_hcs12xe.cmd command file.

 

The next option is using specific unsecure utility from PEmicro:

http://www.pemicro.com/downloads/download_file.cfm?download_id=16

Unsecure_12 Help Files:

http://www.pemicro.com/downloads/download_file.cfm?download_id=14

Note: For downloading is necessary registration.

 

Please look at S12(X) MCU Security document for more details about Security feature at S12XE.

I hope it helps you.

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信