Unique Device ID on MM912J637

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unique Device ID on MM912J637

ソリューションへジャンプ
1,603件の閲覧回数
igw
Contributor II

Hello all,

The data sheet for the MM912J637 has a section describing the MCU Information Register (IFR).  Within this there is an 8-byte entry labelled "Unique Device ID" (see page 395 of the Rev 3.0, 1/2012 data sheet).

 

However there are no details on this ID elsewhere in the data sheet. Just this one mention in a table.

 

Is anyone able to give any more info on this 8-byte ID register?

 

Is it, as it suggests, a globally unique ID?  Is it preprogrammed from the Freescale factory?

 

Bottom line, can I trust it to uniquely identify a particular chip (and hence assembled board)?

 

Thanks,

Ian

ラベル(1)
0 件の賞賛
返信
1 解決策
1,451件の閲覧回数
RadekS
NXP Employee
NXP Employee

Yes, it is really unique ID preprogrammed by Freescale factory. Cannot be changed.

Meaning of bits in this ID is Freescale internal information and cannot be provided to customers.

However this ID contains also production date,....

So, you will newer get two MM912J637 devices with the same ID.


元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,452件の閲覧回数
RadekS
NXP Employee
NXP Employee

Yes, it is really unique ID preprogrammed by Freescale factory. Cannot be changed.

Meaning of bits in this ID is Freescale internal information and cannot be provided to customers.

However this ID contains also production date,....

So, you will newer get two MM912J637 devices with the same ID.


0 件の賞賛
返信
1,451件の閲覧回数
igw
Contributor II

Thank you Radek.  That is just what I needed to know.

0 件の賞賛
返信